Part Number: ADS4246 Dears.
I couldn't find any remark about Isolation in the datasheet (SBAS533D, revised December 2015).
What happens between channels Isolation?
I want to know the Isolation value in the 100Mhz-Band, 200Mhz-Band, 300Mhz-Band, 400Mhz…
Other Parts Discussed in Thread: ADS4246 Dear,
As the ADS4246 is a S&H ADC I would expect a 0 dB flat discrete frequency response, appart from the external input circuit to be considerd. What I want to know: Is there any internal analog or digital implementation…
Other Parts Discussed in Thread: ADS4246 We are in PCB design phase of custom board for Digital Filter. In board, we are using ADS4246 from TI for which there is a requirement of anti-alias band pass filter before ADC sampling. The ADC sampling frequency…
Dear Jim,
TSW1400EVM uses Altera FPGA. I am using Xilinx. Therefore I cannot use it.
I want to ask some questions about SPI configuration.
I can get the correct data when I use TEST PATTERNS. I send the data through SPI as follow:
Input CLK = 50MHz
Address…
Part Number: THS4541 Other Parts Discussed in Thread: ADS4246 , , THS4531 , THS4551 I'm trying to use a ths4541 to drive an ads4246 ADC and am having a problem with the dc levels of the outputs.
The ADC expects inputs balanced about 950mV and outputs…
Part Number: ADS4246EVM
We are using the ADS4246EVM connected to a Xilinx Artix-7 FPGA as a development system whilst our hardware is ready.
As a medical company, we need to make sure the ADS4246 , via the SPI, has been programmed correctly. Therefore, after…
Part Number: ADS4246EVM We are using the ADS4246EVM connected to a Xilinx Artix-7 FPGA as a development system whilst our hardware is ready.
As a medical company, we need to make sure the ADS4246, via the SPI, has been programmed correctly. Therefore,…
Part Number: THS770006 Other Parts Discussed in Thread: ADS4246 DEARS.
I want to use THS770006 and ADS4246. Are there design issues for THS770006 and ADS4246? Help me review the schematic.
Thank you
Other Parts Discussed in Thread: ADS4246 Hi,
I am Ravi Teja Talluri from Alpha Design Technologies Pvt LTD.,
I am looking for some assistance on our design.
Actually we are interfacing the ADC card to Virtex 4 - FX100 FPGA
we have following questions…
Hi,
No cable is needed to connect the ADS4246 EVM to the TSW1200. The connectors used in the two boards do mate up directly. I am told that Samtec will create cabling to connect between their connectors, but that is on a special order basis. We have…