Part Number: ADS4249 Hi
i have Zynq board in which PL bank interface (1.8V) with ADS4249
also using PL SPI with 1.8V but still SPI is Not working with ADS4249
when we write 0th reg with 01 i can see following
but when again i try to read same reg i am…
Part Number: ADS4249EVM Dear TI-
I am working with the ADS4249EVM and TWS1400. Both of these are in the stock/out-of-the-box configuration. I am observing larger than expected spurious in the FFT. Additionally, the codes view appears to have a pronounced…
Part Number: ADS4249 Hello,
My customer is testing reading and writing the ADS4249 registers on a board they designed.
Other registers are read normally with the set values.
Below, 0x4A and 0x58 both wrote 0x01, but board 1 was read as 0x41/0x01 and board…
Part Number: ADS4249 Hello,
My customer is testing a board they designed using the ADS4249.
They say that the reference clock of 245.76MHz is observed at the RF IN port of ADS4249.
In what cases can symptom like this occur?
Is there a way to reduce the…
Hi Massimo,
Correct, the offset should match the ADC input common mode VCM or the adc will overrange and clip. Can you share images or csv data of the channels? Please share both channels with the inputs off and also share both channels with the channel…
Part Number: ADS4249 Hi Team,
A customer is using the ADS4249 IBIS Model and if they check zero transmission line using FPGA as load, signal starting (rising for 700mV), if we connected using transmission path and connected to Load signal rising for…
Part Number: ADS4249
Hello Team,
I wonder the maximum power consumption of IDRVDD. In ADS4249 datasheet, it specifies typical value only.
1. Could you let me know the maximum value? My customer needs this value to see if there's any possibility of overcurrent…
Part Number: ADS4249 Hello,
My customer would like to receive the LVDS output of the ADS4249 on an FPGA.
They found differences in LVDS DC characteristics between the ADS4249 and FPGA, as shown below.
Could the difference between the two DC specfications…
Part Number: ADS4249 Hello,
I have a few questions regarding the differential analog to digital converter ADS4249.
1. UNUSED Pin - should I let this pin float or tie to ground?
2. The ADC has differential inputs (INM, INP), but I have a single ended bipolar…