Part Number: ADS4249EVM Other Parts Discussed in Thread: ADS4249 I am experimenting with different termination impedances on the analog inputs of the ADS4249 using the ADS42xx/58C28 EVM. Sheets 2 and 3 of the schematic (attached) shows the input circuit…
Part Number: ADS4249EVM Dear TI-
I am working with the ADS4249EVM and TWS1400. Both of these are in the stock/out-of-the-box configuration. I am observing larger than expected spurious in the FFT. Additionally, the codes view appears to have a pronounced…
Part Number: ADS4249EVM Other Parts Discussed in Thread: ADS4245EVM , ADS4245 I am interested in evaluating the ADS4245. I cannot, however, locate any stock of the ADS4245EVM. I do locate stock of ADS4249EVM. It appears these two eval platforms are based…
Part Number: ADS4249EVM
Hi,everyone
In the past post, we solved based questions. But there are still some questions about ADS4249EVM.
When I use ADS4249EVM to collect data, there are some high harmonics. The input signal is a sine one with furquence…
Part Number: ADS4249EVM Hi
I want to use TSW1400EVM capture board to collect digital data from ADS4249EVM board.
But when I completed all steps in the user manual https://www.ti.com/lit/ug/slau333a/slau333a.pdf 2.2-2.5, HSDC Pro shows this question.
But…
Guantao, thanks for showing these images.
One suggestion I have is to try it again with the "Device Desc of FTDI Port" set to "ADS4249EVM" and see if this allows you to connect? If not, we can try to look into an alternative solution. Please try this…
Part Number: ADS4249EVM Other Parts Discussed in Thread: DAC3482EVM , ADS58C28 I cannot get the TI GUI to connect to the EVM board to configure the ADC. (The USB status will not turn green even after resetting it) It is not the USB cable or the drivers. …
Part Number: ADS4249EVM I have powered up the board with +5V across J10 and J12.
I am sending a clock signal (0.5V rms sine wave) into J19
by my calculations that gives a 1.5 V sine wave to pins 26 and 27 of the ADC as described in Table 7.3 of the datasheet…
Part Number: ADS4249EVM Other Parts Discussed in Thread: DAC3482EVM I am attempting to build something similar to what is detailed in Application Report SLAA545 , with the same hardware, which I currently have.
The main difference is that I need the analog…
Part Number: ADS4249EVM Other Parts Discussed in Thread: ADS4149 It is connected to ADS4249EVM(TWS12XX_CONNECTOR)-> FMC-ADC-ADAPTER-> Xilinx board.
Can you get the source code for the lvds interface control and register settings? vhdl or verilog…