3808.slwu087d.pdf User,
See section 3.1.2 of the attached HSDC Pro GUI User's Guide for instructions on how to manually download firmware.
Regards,
Jim
3806.slwu087d.pdf Nikunj,
If you are using a coherent IF input, the exact frequency value needs to be entered for the ADC target input frequency. If you are not using a coherent input, you can leave this blank. See the HSDC Pro GUI User's Guide (attached…
Farah,
You need to increase the capture size parameter under the "Capture Option" tab on the HSDC Pro GUI. See section 3.1.3.1 of the HSDC Pro GUI User's Guide for more information regarding this.
Regards,
Jim
5305.slwu087d.pdf
Yuke,
The data format from the ADC can be either 2's comp or offset binary. This is set by register 0x43 bit 0 in page 0x6800. By default, this is set to 2's comp after a reset.
In regards to your other questions, see tables 11 and 13 in the ADS54J60…
Haotian,
We do not have the bandwidth to support you with this effort now. I would suggest you start using the Xilinx help forum on their website or read up on the JESD IP Core document provided by Xilinx (see attached).
Regards,
Jim
pg066-jesd204_v7…
Katherine,
For #1, N' is total number of bits per sample and that would be 16. With M = 1, your equation is now 2048*1*16*10/(8*8) = 5.12Gbps.
For #2, you need to consult with Xilinx. Their JESD204B IP core determines this. See attached for more info…