Part Number: ADS5263EVM Dear Sir or Madam,
Would it be possible to provide us the gerber files of the ADS5263EVM? We need the exact lengths of LVDS lines from the ADC to the Samtec connector.
Best Regards,
Gruffalo
Part Number: ADS5263EVM Other Parts Discussed in Thread: ADS5263 Dear Sir or Madam,
We would like to build a test board with the ADS5263 and control it using the TI test SW (ADS5263EVM GUI).
I am guessing that the EEPROM to the FTDI chip https:…
Part Number: TSW1400EVM Dear Sir or Madam,
Would it be possible for TI to share the FPGA project source files for the ADS5263EVM +TSW1400EVM. We would like to use the TSW1400 and the HSDSC acquisition program together with a "self made" ADS5263 eval…
Part Number: ADS5263EVM Hi, expert,
My customer found there is a 5MHz spur without input, they added a 80MHz input clock.
Could you please help analysis why there is this spur? Thanks.
Best Regards
Chen
Part Number: ADS5263EVM Other Parts Discussed in Thread: ADS5263 Dear Technical Support Team,
Does GUI of TSW1400EVM set the trigger threshold of waveform like oscilloscope?
For example, set trigger threshold at rising some point of sinewave and capture…
Part Number: ADS5263EVM Other Parts Discussed in Thread: ADS5263
The first question is about the memory capacity:
Based on ADS5263EVM+TSW1400, when the signal is sampled through 4 channels at 10MHz, the memory capacity should be 2^30 / (4*2) = 2^27…
Part Number: ADS5263EVM Other Parts Discussed in Thread: ADS5263 Hi,
Using the ADS5263EVM + TSW1400, can I do the following:
Capture a data sequence (ideally 64k in length) from each of the four ADC's inside the ADS5263 on the ADS5263EVM card (such…
Part Number: ADS5263EVM The current user guide for ADS5263EVM is listed for Rev A. I currently have the Rev B design, which looks like it has wired the serial interface to the J8B connector and allows you to jumper between the USB or the connector interface…
Part Number: ADS5263EVM Hello,
Is there any way to preset default control register state without using initialization over SPI ?
Change the power up default values.