Part Number: ADS5294EVM Other Parts Discussed in Thread: ADS5294 , Dear friends,
I am now designing ADS5294 + FPGA Board.
Cound you provide the FPGA HDL Code for TSW1400EVM (ADS5294 ...).
I have ADS5294EVM but, I did not use it.
My email address is yimidi…
Part Number: ADS5294EVM Other Parts Discussed in Thread: ADS5294 Hi Team,
Our customer would like to know if it is possible to configure two ADS5294EVM evaluation module on a single computer.
According to our customer, initially the module consumes 1.224A…
Part Number: ADS5294EVM Other Parts Discussed in Thread: DAC3484EVM , Hi staff Customers require the following specifications for high-speed signal processing:
constructing FPGA-based feedback loop with ADC and DAC feedback bandwidth/signal bandwidth from…
Part Number: ADS5294EVM Other Parts Discussed in Thread: ADS5294 Hi,
One of our customer purchased ADS5294EVM and facing issue with second and 8 channel in ADC.
Could you pls look in to this issue and kindly advice how to proceed further.
Best Regards…
Hi,
Sorry for the delay.
Yes, you should be able to use THS4509 as single-ended to differential converter and to drive ADS5294. See the circuit from the ADS5294EVM user guide below. You can use this circuit as a starting point and then empirically optimize…
Part Number: ADS5294EVM Hi
is it possible that you can send me the PCB /Schematic Design form Evalboard ADS5294EVM,so I can save some time in creating my ultrasonic A/D Device.
thanks in advance
if yes I am using Altium Designer.
Best regards
Part Number: ADS5294EVM Other Parts Discussed in Thread: ADS5294 hi all,
we are facing an issue with the ADS5294 EVM .
The current drawn from 5V supply is only 0.1 A.
it had to be 0.4A.
we also connected the TSW1400 board to ADS5294 we are getting TIMED_OUT_ERROR…
Part Number: ADS5294EVM Other Parts Discussed in Thread: ADS5294 hi all,
we are using ADS5294 EVM with KC705 (FPGA EVM) for data capture
we have terminted the ADC input and captured ADC output data.
we are seeing high noise floor of about 50dB.
Please…
Part Number: ADS5294EVM Other Parts Discussed in Thread: FMC-ADC-ADAPTER , ADS5294 I would like to use the ADS5294EVM and TSW1400EVM to evaluate the performance for our specialized application. In particular, we are interested in the phase stability over…
Part Number: ADS5294EVM Other Parts Discussed in Thread: ADS5294 hi all,
we are workinng with 8 channel ADC = ADS5294
input to ADC is 2MHz and -30dBm from signal generator
the following input channels have issues of high noise floor of about 45dB and contains…