Amit,
The ADS62P49 is a 14 bit device. You should have data connected from pin 35 to pin 9 of J1. If you are using the ADS62P29 12-bit device, connect the data pins from pin 31 to pin 9 of J1. For this family of parts, HSDC Pro uses the MSB's bits when…
Part Number: ADS62P29 Hello,
I asked this question in another post, but since that post started wit ha different topic it would be better to ask again in a separate post.
I sent a sampling clock in burst mode (100MHz, 400+ cycles) to the ADC when a differential…
Part Number: ADS62P29 Hello,
I have got some problems with my ADS62P29EVM and I was wondering if anyone could offer some thoughts. The schematics of ADS62P29 is at
I used the default clock configuration, clock comes from J19. The clock is a 1.5Vpp, 100MHz…
The instructions for Windows 7 don't work on Windows Vista... I followed the instructions. It was slightly different then described, in the way that the driver installed by himself, after that I wanted to update the driver with the one from FTDI, but…
Other Parts Discussed in Thread: ADS62P29 , LMK03806 hello,everyone,
I am trying to do some evaluation on ads62p29 EVM_rev_C board.
This is what I got from the DDR LVDS interface.RX_OUT_oddl[11:0] is the signals from the ADC's LVDS after the DDR_LVDS…
Other Parts Discussed in Thread: THS4509 , ADS62P29 , ADS62P28 , ADS62C17
Hi, I have encountered a problem while working with ADS62P29. My application consists of THS4509 amplifier, ADS62P29 ADC and Spartan 6 FPGA. ADC is sampling baseband signal (0-15 MHz…
Other Parts Discussed in Thread: ADS62P49 , ADS62P28 , ADS62P29 , ADS62P48 , ADS6424 , ADS4249 , ADS62P24 Are there any other pin-compatible options for the ADS62P48 ? I am interested in an alternate ADC that will have lower low-frequency noise, ideally a chopper…
Hi
The I received firmware file is not including AFE5801 I want to use.
When I look at the firmware, it's version info is `define FIRMWARE_VER 8'd2 // Rev 2 6-10-12
Device list is as below,
Which I have to select one of them for AFE5801?
`define…
Other Parts Discussed in Thread: ADS62P29 I am designing a system around the ADS62P29. The outputs of the ADC essentially have a DDR LVDS setup in which when the clock is high Dn is output on the pins and when the clock is low, Dn+1 is output. What component…
Thank you for your reply Jim. Sorry for the delay on my end, as I only have time to work on this project on weekends.
Anyway, the linked files do work. Subbing in the attached .rbf for my generated .rbf causes the ADC to no longer work. So, the only answers…