Part Number: ADS7052
Hi Team,
I have two questions about supply current of ADS7052.
Supply current is shown on datasheet as below.
Do you have IDVDD for DVDD=3.0V?
Does the line marked in yellow mean that CS and SCLK have a significant impact on the consumption…
Part Number: ADS7052
Hi Team,
Could you kindly help to check whether the SCH is ok?
If the SCH is ok, I would like to ask further questions.
Customer do the following three lab test, totally test 5 samples .And after the third test, one of the 5 samples…
Chen,
This algorithm used in that GUI is not a prominent one, and is not recommended. It was a result of a necessity, and we do not commonly use it.
I suggest to use the more widely known methods instead.
Regards
Cynthia
Part Number: ADS7052 Other Parts Discussed in Thread: REF1933 Hello TI member :
I am trying to build a 14 bit environment by using ADS7052, could you help me to confirm whether my calibration flow was wrong or correct ?
My test flow are showed below…
Part Number: ADS7052 Hi Team,
My customer use ADS7052IRUGR and found that it works abnormally when the temp is lower than -14℃.
Test environment: Thermometer box, which could keep temp to -25℃~0℃
Test method: Provide 2.048V DC signal to the input of ADS7052…
You are correct, an input op amp might not be needed at those low frequencies
1. The ADS7052 digital output communication pins are pulled high to the DVDD voltage; the input digital pins will use DVDD voltage as the reference voltage for the device to…
Part Number: ADS7052 Hello TI,
I studied SPI communication in ads7052 ADC Converter. I try to communicate with this ADC, by reading for 24 clocks after I set the chips selelct low, but I get only FF. Is there any reason?
I use Clock Polarity Low and…
Part Number: ADS117L11 Other Parts Discussed in Thread: ADS7052
Used in single power supply, low-speed mode. The specification sheet states AVDD1 to AVSS, low-speed mode 2.85 5.5V, Is it possible to use AVDD1=AVDD2=IOVDD=+1.8V, AVSS=DGND=GND(0V)?
Part Number: ADS7057EVM-PDK Other Parts Discussed in Thread: ADS7057 , , ADS7056 , ADS7052 Hi,
We are using a ADS7057EVM-PDK to evaluate ADS7057 ADC. The EVM is connected to a PC through a PHI module. The data is acquired using ADS704X-5XEVM-PDK-GUI installed…
Hi Amelie,
are you sure the LMV321 is fast enough to drive the ADS7052 properly? The datasheet of ADS7052 shows a 200MHz OPAmp at the input of ADS7052:
Also, R64 must be chosen very carefully to not only keep the driving OPAmp stable but to also allow…