Part Number: ADS7066EVM-PDK Other Parts Discussed in Thread: ADS7066 Hi,
I have a question regarding ADS7066. I connected the evaluation board of this ADC, when I wanted to have a maximal sample rate of 250ksps, the SCLK couldn't be lower than 60MHz.…
Part Number: ADS7066EVM-PDK Other Parts Discussed in Thread: ADS7066 Hello,
Is there a GUI for the PAM that runs locally, or is the GUI only on the cloud?
Thank you,
Scott
Part Number: ADS7066EVM-PDK Other Parts Discussed in Thread: ADS7066 I am using the evaluation board of ADS7066, and when I connected it to a signal generator and tried to drive a DC voltage, I got non accurate measurements at the GUI. the left column…
Part Number: ADS7066EVM-PDK Other Parts Discussed in Thread: ADS7067 , ADS7066 Hi,
I have the Evaluation board of ADS7066, and also I have ADS7067.
I wanted to ask if it is possible to still use the TI GUI after replacing these two ADCs on board?
does it…
Part Number: ADS7066EVM-PDK I'd like to drive the ADS7066EVM SPI using my own MCU and not the PAM. What is the easiest configuration to achieve this?
My thought was to separate the PAM and EVM boards and only connect the four pins labeled 5V, 3V3, and…
Part Number: ADS7066EVM-PDK Hi there!
Recently got the ADS7066EVM-PDK and I can't seem to communicate with it. I tried both USB cables that came in the box, and the interface keeps telling me that I have no serial ports available. I checked Device…
Other Parts Discussed in Thread: ADS7066EVM-PDK Hello,
I am looking for a suggestion in selecting a suitable ADC evaluation kit with a USB (with SPI) interface. I would prefer having a 16bit ADC.
I want to perform some real-time processing with a signal…