Part Number: ADS7138-Q1 Tool/software: Dear sirs,
I would like to confirm if the "Data setup time" in the table below refers to the time that the transmitter must satisfy when sending data. If so, does this mean I need to check the actual Data setup…
Part Number: ADS7138-Q1 Tool/software: Hi,
I have AIN7 connected to 5V with a 4.12K in series to sense power supply voltage 5V.
Its that okat. iam concerned on exceeding AVDD+0.3V rating on datasheet.
I have 1.2mA flowing through, i sthat a pro…
Part Number: ADS7138-Q1 Other Parts Discussed in Thread: ADS7138 , ADS7038 Tool/software: Hi,
Could you please send me the example code for ads7138qrterq1 to receive the data via I2C,
I will use the I2C to get the three Voltages ( temperature reading…
Part Number: ADS7138-Q1 we are using the device ti adc 1738 12bit SAR
Hi,
parameters used
1)clock setting =0 2)speed setting=0 3)vref =3.3V 4)manual mode
problem noticed 1) positive offset of 25mv maximum
2) The ADC read value is not…
Part Number: ADS7138-Q1 Other Parts Discussed in Thread: ADS7138 Hi Team,
In ADS7138-Q1,
If we connect the ADDR pin to DECAP pin with a " 0 ohm ", may I know the leakage current through ADDR pin?
Datasheet didn't mentioned about it and we need…
Part Number: ADS7138-Q1 Hi Team,
For ADS7138-Q1, although our ADC input is not a fixed value so using TUE(Total Unadjusted Error) might not reflect the actual performance.
But customer want us to evaluate the maximum error range, based on below…
Part Number: ADS7138-Q1 Hi Team,
From the datasheet description, we try to reset the bit " CRC_ERR_IN " by write "1" to it.
Customer report that the status is still the same after writing "1" to it.
1. I would like to confirm whether writing…
Part Number: ADS7138-Q1 Other Parts Discussed in Thread: ADS7138 Tool/software: Hi
Our current system design uses three ADS7138 ICs, but during the low-temperature test, we found abnormal readings from one ADS7138 on one of the boards. The failure rate…