Part Number: ADS7138-Q1 Other Parts Discussed in Thread: ADS7138 , ADS7128 , BP-ADS7128 Hello team,
My customer has use the ADS7138-Q1 in their ADAS system in A sample, while they are waiting the board, they want to use the EVM board to start the software…
Part Number: ADS7138-Q1 Hi, TI Support Team
The following inquiries have been received from customers.
[condition]
AVDD: 3.3V
Ainx: max. 3.3V
The product is being used under the above conditions, but the spec written in the datasheet is confirmed…
Part Number: ADS7138-Q1 I have configured autonomous mode in our ADC and threshold for each pins are written in respective registers using I2C write operation.
Test case1: To verify the alert pin functionality, I have changed the threshold value for…
Part Number: ADS7138-Q1 I'm trying to communicate with the ADS7138-Q1 over I2C, specifically read from the GPIO pins. In my schematic R1 to the ADDR pin is 33k, therefore the 7bit address should be 0x15h. The device address I've been using is 0x2a (left…
Part Number: ADS7138-Q1 Hi,
Are there driver's or examples available to create a Labview or Python interface for the TI ADS7138-Q1 Automotive ADC with I2C ? Thank you.
Part Number: ADS7138-Q1 hi, if some of GENERAL_CFG registers are not used, do you recommend to keep the bits to 0?
what is possible concern if those are changed to 1? (like increased Iq?)
Part Number: ADS7138-Q1 Hello TI team
I am facing a weird problem with this ADC. AVDD=DVDD=3.3V. and i got the same digital code for the following range of AIN:
50mV<=AIN<=250mV. The digital code related to that range is: 0xD20. From 250mV to 3.3V…
Part Number: ADS7138-Q1 Other Parts Discussed in Thread: ADS7128 , , TLA2518 , TLA2528 , ADS7028 , ADS7038 , ADS7138 Hello,
I would like to know if the ADS7138-Q1 is made with the same die (chip) as the ADS7128?
Best regards,
Denis GALLARDO
Part Number: ADS7138-Q1 hi, Is it possible to contradict the status bit and configuration bit?
for example, the below happens at the same time.
SYSTEM_STATUS SEQ_STATUS is 0b SEQUENCE_CFG SEQ_START is 1b
If this could happen, what is possible reason…
Part Number: ADS7138-Q1 Other Parts Discussed in Thread: ADS7138 hi,
when do Single Register Read or R eading a Continuous Block of Registers, i s it allowed to do NACK from the host at the red circle below? any concerns?