Other Parts Discussed in Thread: OPA2227 , ADS7229 , OPA227 , TINA-TI Dear TI Support,
I am writing you regarding the circuit which consists of 16 independent acquisition channels each one having an Input multiplexer, a conditioning stage (OPAMPs) and an…
Part Number: ADS1274 Hi to all!
Can I work with ADS1274 and MCU with Quad SPI?
This way:
ADS1274 MCU
DOUT1->>>IO0_QUAD_SPI
DOUT2->>>IO1_QUAD_SPI
DOUT3->>>IO2_QUAD_SPI
DOUT4->>>IO3_QUAD_SPI
I need to get data same…
Hello experts
I am looking for a ADC chip set with 16 bit or 24 bit resolution
with on chip capture buffer/FIFO of 1024 samples and it must have a interrupt line
this interrupt line which only interrupt the ELB-REV4 (AM335X based device) once capture…
Analog inputs (12 channels Single Ended) driven through Buffer amp.
Do I still need one more buffer amp stage between MUXOUT and ADCIN as your recommendation? Schematic attached.
ADC input range is 0-5V, as per your recommendation tied VREFP pin to…
Hi Joseph
Thanks for the reply.
Regarding TVS diode, there is an another 5V Reveres breakdown voltage TVS diode , SMF5.0A parallel to ADC_IN pin at battery connector end. And I am sure that there is no issue with the i2C read and write since it worked…
Other Parts Discussed in Thread: ADS1262 , REF5050 , ADS124S08 , ADS1234 Hello Bob,
Thanks for the quick responses you had provided me. I would like to design a moisture analyzer with the given specification below
Maximum 600 g, Resolution = 0.01 g (if Possible…