Part Number: ADS7864 I would like to receive data from 6 channels continuously. The ADC is controlled by the FPGA. Connects four ADS7864s to one FPGA. To do this, you need to minimize the number of control pins connected to the FPGA.
Can I save 3 pins A0…
Other Parts Discussed in Thread: TLV5614 , ADS7864 , TLV2548 I need to download the IBIS model for theAD,DA convertor for a simulation of my prototype circuit board.
I checked it on TI homepage , but the link of ibis model was not described.
If you have…
Part Number: ADS7864 Hello TI Support Team
Is the ADS7864Y/250G4 part a problem when used in an environment of radiation "3Gy"?
If there is no problem, please give the radiation resistance evaluation data.
Thanks n regards
ZHEN
Part Number: ADS7864 Hi
In my appliaction I have a continuous hold sequence (A,B, C, A ...) , address lines are tied to 1 (FIFO mode) but I delay reading data until a certain number of hold signals was given out.
The questoin is what happens to the FIFO…
Other Parts Discussed in Thread: ADS7864 HI! when I use the ADS7864 at the first time, I forget that its input voltage range is between -2.5V and 2.5V and I input 5V .So the output data is all the same wheter i input 5V or 0V .However, I can see the BUSY pin…
Other Parts Discussed in Thread: OMAP-L138 , ADS7864 Hi,
I am looking for a possibility to interface 6 channel ADC with UPP interface of OMAP-L138 EVM. My requirement is to use at least 12 bit ADC with sampling rate 6 MHz.
Can UPP handle 12 bits x 6 MHz…
Other Parts Discussed in Thread: ADS7864 , ADS7846 today, i want to the beagleboard-xm support touchscreen,i refer to some blog,but now ,linux kernel start ,then error with touchscreen ,the ads7864 is the controller of touchscreen.
the error is :
9.669769…
Hi,
The ADS8528 requires bipolar supplies as you described. Other simultaneous SAR ADC's are available; although they are not equivalent. The ADS7864 is a 500kHz, 6 channel simultaneous sampling ADC with fully differential inputs running with 5V supply…
Other Parts Discussed in Thread: ADS7846 , ADS7864 now ,i get some problems about bb-xm with touchscreen,theuboot (2010-12) linux kernel 2.6.32 from modified dvsdk4.0.1.
the main core problem is :
linux kernel start ,but it can not detect touchscreen ;i…
Joe,
We want to use a 6-channel ADC like ADS8558 or even ADS7864. I think the chip select (CS_) can be pull-low all the time. The RD_ (read) signal can be driven by the other uPP channel to control the ADC and drive the clock input of the uPP at the…