Other Parts Discussed in Thread: ADC081C021 , ADS7041 , ADS7888 Hello,
I want to sample the analog signal entering an external ADC IC such as ADC081C021 with a trigger signal from either MCU or other circuitry.
As an example, let's say there is a comparator…
Other Parts Discussed in Thread: ADS7888 Hello,
With regard to the ADS7888, ViL is not specifiedfor VDD below 3V, but the device can operate from a VDD as low as 2.35V. Is the specification for ViL at VDD=2.5V available?
Also, is IiL and IiH available? …
Other Parts Discussed in Thread: ADS7888 , TLV571 Hi,
I would like to use an ADS7888 ADC, with a conversion rate of 1MSPS, and interface it with an 8Mhz microcontroller. I understand that I cannot connect the ADC serially to the micro, since the ADC is…
Other Parts Discussed in Thread: TLV5624 , ADS7888 Hi,
We are thinking to interface ADC and DAC using C5505 I2S. Since we have multiple ADC/DACs on board, One ADC and DAC might need to be connected to the same I2S port. Does anyone know if the C5505 I2S…
Hi Shinichi
We do not have IBIS model for ADCS7476.
We do have pin to pin replacement for ADCS7476 which is ADS7886. This is 12 bit 1MSPS SAR ADC with same package and pin out as ADCS7476. We have IBIS model available for ADS7886 and can be found at …