Part Number: ADS7924 Dear Team,
I have some questions about ADS7924IRTER. Please help answer them as soon as possible. Thank you.
1) What is the input voltage range of CH0, CH1, CH2, and CH3 pins? Do Figure 1 and Figure 2 conflict? (As shown below) 2…
Part Number: ADS7924 Other Parts Discussed in Thread: AM2434 , I have several prototypes made using ADS7924 and an AM2434 talking to the ADC over I2C.
I am sending a soft reset command to the ADS7924 via I2C at start of initialisation.
On some chips (but…
Part Number: ADS7924 Hi team,
I just want to confirm the any requirement of power up sequence because there a few information in the datasheet.
The requirement is only below? Is there any timing requirement?
AVDD must turn on before DVDD(always AVDD>…
Part Number: ADS7924 Hi,
Iam trying to implement I2c master code with communicating with 2 ADS7924 slaves.
I Followed the below writing and reading method.
For writing i send the below data for the 1 ADS7924 with slave address (1001001)
1.To wake up the…
Part Number: ADS7924 Hi,
I am using ADS7924 in my application for voltage monitoring and protection.
I want to know what happens when switching between the modes, for example while running in Auto-Scan mode, If the mode is changed to Manual scan mode…
Part Number: ADS7924 Hi Team,
My customer is having an issue with the ADS7924 in that only CH0 reading is matching the real measurement.
The following were the I2C communications between the host PC to the ADS7924, used Manual-single mode.
Host PC reads…
Part Number: ADS7924 Does the ADS7924 have any startup timing requirements for the reset pin wrt the power supplies? I don't see anything in the datasheet.
Thanks,
Nick
Part Number: ADS7924 Dear Team,
My customer is considering to add an OpAmp between MUXOUT and ADCIN of ADS7924 to improve sensing performance. The ADS7924 datasheet describes about the RC filter setting at "8.1.2 Using an Operational Amplifier and RC…
Part Number: ADS7924 Hi.
I'm trying to run ads7924 using stm32f series.
But i2c does not work so I check the i2c line.
Between 0R, MCU side 3.3V but ads7924 side 0V. I set pull up setting of MCU internally .
What is the problem? below is the circuit…
Part Number: ADS7924 Hello Guys,
Our customer is having some unexpected i2c behavior with a ADS7924IRTER. It is supposed to respond to the address of 0x48 but he is only getting acks at 0x28. it is only responding with acks at address 0x28. See attached…