Part Number: ADS7945 Other Parts Discussed in Thread: REF5030 , ADS7946 Hello,
I am simultaneously sampling two differential signals with tho ADS7945s sharing a single chip select. I would like to use a single REF5030 to drive the reference input of both…
Part Number: ADS7945 Hi Bros,
When I using ADS7945EVM, I cannot find our SCH in the user guide. It is inconvenience. Could I have the ADS7945EVM's SCH?
Also, customer want to connect their board's ADC to our EVM so that they can read the data from…
Part Number: PGA113 Other Parts Discussed in Thread: OPA320 , OPA357 , ADS7945 , ADS7946
Hello to whom this may concern, This is the description of the situation: 1. Input ignal: The system need to be able to capture two types of signal (from a BLDC or PMSM…
Other Parts Discussed in Thread: ADS7945 HI my customer would like to use two ADS7945 in parallel.
He would like to read both measurments at the same time and would like to know the jitter between both measurments.
could you please help?
regards
kamal
Other Parts Discussed in Thread: ADS7263 , ADS7945 The part ADS7945SRTER is defined up to +125 degree in most on-line shops and in your own technical specification document. Nevertheless on your web-site it is specified only up to +85. Could you please…
In the description of the 32-clock frame the datasheet shows a 33rd clock pulse before beginning a new conversion. I would like to know if I could begin a conversion immediately after the 32nd clock. Will this work?
Part Number: ADS7946 Other Parts Discussed in Thread: ADS7945 Tool/software: Code Composer Studio Hello, TI's Engineer,
Problem description reference voltage is 2.048v
Demand: two signal inputs, POS signal range 0-2.048v (VREF); CMD signal range 0…
Part Number: ADS7946 Other Parts Discussed in Thread: ADS7945 , For SNR & SINAD performance @ 2 MSPS the data sheet lists performance only at 20 KHz input frequency. Are there plots for these out to Nyquist frequency (~1 MHz)? I would like to see how…
Hi Mehmet,
yes, the ADS7945 can be connected in this manner because it provides true differential inputs. But the ADS8586S needs the "AIN_nGND" pin to be connected to signal ground which is not possible in combination with the ISO224 because both outputs…