Part Number: ADS7952 Hello expert,
Do we have NCT7201Y replaced solution? It is 8-ch/12-bit ADC general purpose voltage monitor. Thanks a lot!
Best regards,
Ann Lien
Part Number: ADS7952 For ADS7952, what are the AC voltage (dynamic) limits on the SCLK pin and what is the safe duration for which the AC voltage (dynamic) can be applied.
The datasheet only mentions the absolute maximum for DC voltage of 0.3V.
Regards…
Part Number: ADS7952
Hi colleagues,
the power supply and reference setting of ADS7952:
--
we use 2xVref (2.5V) for a 3.3V power supply system, now we test our demo with this condition and input voltage is lower than the 3.3V power supply (below 3V).
the…
Part Number: ADS7952-Q1 Dear Sir:
Regarding the ADS7952-Q1 Issue.
1. MULTIPLEXER :CH0~ CH11.
No Use channels. It can float these pins.
Is it correct?
2. NC PINS: Pins(Pin11~14) internally not connected, do not float these pin
It needs to connect the…
Part Number: ADS7952 Hi Engineers from TI,
ADS7952 with QFN package, we measured SCK CE MISO, all waves right compare with Mercury system, but MOSI signal without channel information.
So could you give us any suggestions?
Thanks
Hongjin
Part Number: ADS7952-Q1 We are doing a production run of one of our products. This particular design calls for the ADS7952SRHBT, however it is out of stock everywhere and extremely difficult to find. The ADS7952-Q1 is available. Apart from the package…
Part Number: ADS7952
I have an ADS7952 connected to a PIC32MZ using SPI communication (3.3V IO) with all 12 channels connected to current monitor voltage outputs (0-5 V). For referance, the +VA = 5VDC; +VBD = 3.3VDC; Vref = 2.5VDC; MXO is tied to AINP;…