Part Number: ADS7953 Hi team,
could you help with below question for ADS7953?
is it necessary to use LDO to power VA/VBD/VREF? can we use the DCDC to power? and can we use one rail for these pins?
Part Number: ADS7953 The datasheet's Figure10 shows that the current increases as the sampling rate increases.However, the test found that in the power down mode, the current of the chip VA was very small. Even if the input clock speed was changed…
Part Number: ADS7953 I have ADS7953 and ref4132-3.0v.
The power supply voltage of my system is 5V and the reference voltage is 3.0V.
If the ADC input signal is 4.0 Vpp,
I have problems for these 2 cases
1) 1xVref
Does digital output is full scale 0xFFF…
Part Number: ADS7953-Q1 Hi team,
Could you tell me the analog input maximum value? In my understanding, this max value is 5V even in both range1 and range2. Ultimately, I'd like to check if this ADC can observe 12V signal directly.
Best Regards…
Part Number: ADS7953 What is the ideal power up sequence for power supplies: +VA and +VBD?
Is there a power sequence requirement for +VA and +VBD regarding to which one should come up first? or does it not matter ?
Part Number: ADS7953 Other Parts Discussed in Thread: ADS1278-SP , ADC128S102QML-SP , ADS1282-SP Hello,
Is there a space version of your ADS7953SBDBTR? If not, is there another 16-ch 12-bit part that is space rated?
Thanks, Adam
Part Number: ADS7953-Q1 Other Parts Discussed in Thread: ADS7953 Hello,
I plan to use the ADS7953-Q1 with a digital I/O supply voltage of V(+VBD) = 1.8 V.
Datasheet SBAS652A (for ADS79xx-Q1, August 2014) specifies the Low logic-level input voltage VIL to…