Hi ,
I am using ADS7958SRGET in my design. I have few queries listed below.
1. Is it possible to power-up the device via in-band signalling (SPI Frame) ?
2. Can system-level soft-reset be asserted (via in-band signalling) ?
3. If the control registers…
Other Parts Discussed in Thread: ADS7958 , ADS7948 About the Min value of SCLK and sampling frequency of ADS7958, if there is information, please let me know. ※Only the Max value was indicated to the datasheet.
Thank you for your consideration.
Other Parts Discussed in Thread: ADS7961 , ADS7958 Hello,
We have started working ads7961 on board.
on reading channel 9any channel) I always get up to 7bit scale , but no more than that.
for example:
for channel 0: 0x07E0
for channel 1: 0x17E0
for channel…
Hi Vishy,
the problem was caused by a wrong description of the ADC in the device tree. See the following binding:
* Texas Instruments ADS7950 family of A/DC chips
Required properties:
- compatible: Must be one of "ti,ads7950", "ti,ads7951", "ti,ads7952…
Part Number: ADS7953 Hello,
I am using the ADS7953 and have a question regarding the use of GPIO2 to control the input range. The input range can be selected via GPIO2 or bit DI06 in the mode control registers. What happens if GPIO2 is used to select…