Part Number: ADS8028EVM-PDK Hello,
I could not find the board layout information in the User guide document. It would be very helpful if the same can be shared.
Thanks and Regards,
Sufyan Khan
Part Number: ADS8028EVM-PDK Hello,
I working on the ADC evm kit without the MMB0 motherboard and using an external microcontroller. The kit is working fine but I wanted to increase the range of analog inputs. As per the datasheet, the range is set to…
Part Number: ADS8028EVM-PDK Other Parts Discussed in Thread: DAC81416 , ADS8028 , DAC81416EVM Hi all,
We have two EVBs: ADS8028EVM and DAC81416EVM. And we have one SPI master. The question is, can these boards share the MISO signal wire directly? As shown…
Part Number: ADS8028EVM-PDK Other Parts Discussed in Thread: ADS8028 Hi,
We have an ADS8028EVM-PDK board. And the SPI signals of the ADC EVM is connected to the external microcontroller. Whereas we want to use the power supply from the MMB0 board. As…
Hi Andreas,
If you look through the ADS7038EVM-PDK Users guide , you will find a layout that is very similar to what was used on the original ADS8028EVM. There is a single GND plane with the digital tracking routed away from the analog inputs. Bypass AVDD…
Other Parts Discussed in Thread: ADS8028 , ADCPRO Hi,
When trying to install MMB0 with ADS8028EVM in windows 8, the installer doesn't complain, but when I am looking in device manager I see that there is an unknown device on USB fabric, VID 0x0451, PID…