Part Number: ADS8328
We are driving the analog input of the ADS8328 with an instrumentation amplifier being powered by +/- 7VDC. The SDC is powered by a separate 5V supply. There is also a passive LPF on the input consisting of a 10K resistor and a 10nF…
Part Number: ADS8328 Hello, I am experiencing the same issue as discussed on TI forum here . I am using Particle Xenon (nRF52840) running Arduino bootloader. I have the code running to write into CFR and read the data back, switching channel and then reading…
Part Number: ADS8328 Other Parts Discussed in Thread: REF3425 , Hi,
I am using the part :ADS8328. In my design we are having 2.8V rail. I would like to know whether can I use REF3425 to provide a reference voltage to my ADS8328? I am more concerned…
Part Number: ADS8328 Hi, I'm using the ADS8328 in a design that has separated grounds at the client's request, and the ADC (ADS8327IBPW) seems to be shorting the analog and digital ground nets.
Based on the datasheet, the connections I'm using seem…
Part Number: TMS320F28335 Other Parts Discussed in Thread: ADS8328 , C2000WARE Can I get an example of SPI communication between tms320f28335 and ADS8328?
Part Number: ADS8328 I'm using the ADS8328IBPW at VA=5V, VBD=5V, REF+=4.096V, REF-=0V with CFR at the default values, notably Auto Channel Select enabled, Manual Trigger, EOC active low, etc.
I'm getting very poor DC isolation between +IN1 and +IN0…
Part Number: ADS8328 Other Parts Discussed in Thread: ADS1220 I have problem with ADC ADS8328IPWR. The problem is show up then I am reading the CFR register and data, so as to interpret correctly the CFR and data I need to perform bit shift down . Thus I…
Sorry Jake,
Guess I noticed the 1864 device which shares a datasheet. Unfortunately that makes things tougher. Our ADS8328 or ADS8330 might work for you but the pinout is different. We don't have anything in the 10-pin MSOP lead frame.
Other Parts Discussed in Thread: TMS320F28335 , ADS8328 , TEST2 I have an ADS8328 hooked up to the McBSP of my TMS320F28335 and am using it to read in from two different audio sources. I have designed a small library that initializes the device into Manual…