Part Number: ADS8345 Other Parts Discussed in Thread: ADS8344 ,
I have an evaluation board including a Cortex M4 MCU from a different vendor. Board has VDD = 3V3 , GND, 5V, DAC. As you guess I don't have different ground planes such as DGND, AGND. …
Part Number: ADS8344 Hi,
Good Day.
What is Minimum Relative Accuracy (LSB)? (I assume this means the lower number is more favorable on the NB part as the accuracy is correct to within 6 LSBs instead of 8 LSBs. Is my interpretation correct?
What is meant…
Part Number: ADS8344 Hi team, Does ADS8344 have a calibration function? Abnormal values were first observed, but then returned to normal values. If it does not have a calibration function, are there any possible factors in the first measurement error? Sincerely…
Part Number: ADS8344 Other Parts Discussed in Thread: ADS8354 Hello,
My customer has a question for ADS8344.
The datasheet says that clock mode should be set before setting to power-down mode(PD1=PD0=0) when power is first applied.
In the customer’s…
Part Number: ADS8344 Hello there,
I would appreciate if someone could help me with an issue I have. I am using ADS8344 to sense several signals from photodiodes. The signal is coming from a standard photodiode amplifier based on an OPAMP. At the OPAMP…
Part Number: ADS8344
Hello, I'm working with ADS8344 to convert analog data coming from a sensor.
ADC is connected to a uC and communication goes through SPI interface (2MHz clock). ADS8344 is set up in external clock mode, and in single ended channel…
Part Number: ADS8344 I am reading 4 channels at a time from the ADS8344EBG4 in 24-bit mode, with no power-down between cycles, using an external clock ( 1.5 MHz )
In this mode I send ( 13 * 8 ) clocks to the device, with nCS framing all of the clocks…
Part Number: ADS8344EVM Other Parts Discussed in Thread: ADS8344 , Hello
I'm trying to connect ADS8344 EVM with ATMEGA128.
But I'm not sure how to config for the Power, GND and lots of Fuses.
Please let me know which setting is correct once external…
Part Number: ADS8344
Hello team,
Hope you are doing. Have a customer who is requesting clarification on 'pitch' for this part as datasheet does not have information on DB package:
We just have conflicting TI datasheets… one says .635mm, the…