Part Number: ADS8354 Other Parts Discussed in Thread: TMS320F280049
Hello,
I have a microcontroller, that communicates with an ADS8354. I want to change the configuration to:
RD_DATA_LINES = 1,
INPUT_RANGE = 1,
REF_SEL = 1.
Therefore I have to send the…
Part Number: ADS8354
Hello,
I am trying to set internal reference voltage of ADS8354, but I am getting unexpected behavior from the IC. Any help would be appreciated.
Here is what I tried : Settings : - I am using 48 falling edge clock/ 3MHz using…
Part Number: ADS8354 I am currently trying to run only one channel of ads8354. I am communicating through STM NUCLEO Board with adc.
REFERENCE VOLTAGE FOR BOTH CHANNEL IS GIVEN FROM OUTSIDE.
REFIO_A=REFIO_B=5V
REFGND_A=REFGND_B=0V
AVDD=5V
DVDD=3.3V
INPUT…
Part Number: ADS8354 Other Parts Discussed in Thread: ADS8353 Dear team,
My customer consider using ADS8354 at their application. but there is issue of ADC output. please review below status and let me know your opinion.
<Setting>
- For CFR.B9 …
Part Number: ADS8354 The part states for the +/-Vref input range that the common mode voltage should be Vref/2 while for +/-2xVREF the CMV is Vref. For a 5V analog rail the Vref VCM makes sense with +/-2xVref input range because Vref/2 VCM at 1.25V would…
Part Number: ADS8354
Hi,
i have some problems receiving the SPI data from the ADS8354 correctly. The recieved bits are shiftet by one so i would quess it is a problem with CPOL & CPHA but i tried all combination and had no luck.
Based on the timing…
Part Number: ADS8354 Other Parts Discussed in Thread: THS4521 , ADS8353 Hello,
I was wondering how to terminate the the negative input when using single-ended input signal?
Thanks & regards,
-albin
Part Number: ADS8354 Other Parts Discussed in Thread: OPA2350 , THS4522 1. I am trying to follow the recommended operating conditions of the ADC, with AVDD set to 5[V] and DVDD set to 3.3[V]. I am confused as to where to connect the ground of both power…
Part Number: ADS8354 I would like to use the ADS8354 but not at it's full throughput capability. I want to use the device in the 32-CLK, Single-SDO Mode. The datasheet timing table "32-CLK, Single-SDO Interface Specific Timing" indicates a minimum spi…