Part Number: ADS8363 Hello,
I am using this ADC on my board with the device configured to use only one shared reference (REFIO1) for both internal ADCs on the chip. The resulting data was extremely noisy to the point that we were only able to use 12 bits of…
Part Number: ADS8363 Hello,TI data converter experts:
We are using ADS8363 for two channel simultaneous sample.We use a FPGA to drive ADS8363,the problem we are facing is that sometimes when powering up ADS8363 load error and get wrong data,typically…
Part Number: ADS8363
Hello team,
If my customer wants to use ADS8363 with 0-5V SE input,
CMA pin should be connected REFIO or 2.5V. Is this right?
Do they need to connect (-)input with REFIO or 2.5V?
Or both connections must be required?
Best Regards…
Part Number: ADS8363 Hi team,
My customer has a question regarding the full-clock mode of ADS8683.
When the IC /CS signal is enabled, there is a rising edge of CONVST, but SDI and RD seem to be ignored and take no action according to the pin function, and…
Part Number: ADS8363 Other Parts Discussed in Thread: ADS8584S Hi Team,
Could you please comment if ADS8363 will be able to simultaneously sample 4 inputs?
From the DS it looks like it can only sample 2 channels simultaneously.
What ADC would you suggest…
Part Number: ADS8363 Other Parts Discussed in Thread: OPA2365 Hi
My circuit is below, R233 is a NTC thermistors, -10℃ R233 is 275.8Kohm, 25 ℃ R233 is 50Kohm, 70℃ R233 is 8.663Kohm.
When I use ADS8363 sample ADC_TEM, when environment temperature lower…
Part Number: ADS8363ADS8363 is differential input ADC IC.
but, when I use this ADS8363, It has to use differential input Opamps in front of ADS8363 input.
Why differential opamp should be in the input? is this neccesary?
I want to design circuit without…
Part Number: ADS8363 Hi
We are using ADS8363 REFIO1 and REFIO2 as recommended in manual, connected to a 22uF capacitor directly on pin.
We are sending the device command to enable REFIO output and set it to 2.5V
What we are seeing is an extremely low…
Part Number: ADS8363 Other Parts Discussed in Thread: THS4561 , THS4531 ,
Hi team,
This is my customer design. Could you pls help give any comments? Below are what I found,
1. Leave CMA/CMB pins open, as it is as full differential input use case;
2. Demount…