Part Number: ADS8588H Other Parts Discussed in Thread: TINA-TI Dear Sirs
I am looking for a Pspice Model for ADS8588H if possible.
Thanks a lot and Regards
Sal
Part Number: ADS8588H HI Sir
I want to design a 3 phase meter & poly meter
I choose the ADS8588H for 3 phase monitor---> did you have any source code for Survey?
another project is poly meter-->did you have any suggestion?
thanks
Part Number: ADS8588H Hi,
what is the output voltage of REGCAP1 and REGCAP2? This is not specified in the datasheet, but needs to be clarified for selection of capacitors with appropriate voltage rating.
Regards,
Matthias
Part Number: ADS8588H Hi,
in the datasheet it's said "In order to maintain the dc accuracy of the system, matching the external source impedance on the AIN_nP input pin with an equivalent resistance on the AIN_nGND pin is recommended"
…
Hi Sebastian,
Sebastian Wue said: That raises the question for me, what value to use for full scale 5V, 10V or 20V?
I would read this blog about converting from code to voltage and the explanation of the FSR.
[Blog] It’s in the math: how to convert an…
Part Number: ADS8588H Other Parts Discussed in Thread: INA188 , TMUX6219 , OPA2197 , TMUX6236 Dear TI,
We need a programmable Gain amplifier which should have gains of 10 and 50,
input to ADC AD8588H is being fed from current transformer, and we want PGA…
Part Number: ADS8588H Other Parts Discussed in Thread: REF5025 hello Ti,
We are using ADS8588H on our board,
i have selected the input range to +/10V, by configuring pins RANGE = 1 and STBY = 1,
i applied 2.616Vrms,( Vp =3.69Vpk),50Hz signal to ADC and…
Part Number: ADS8588H
Hi,
According to the datasheet "The device must always be reset after power-up as well as after recovery from shut-down mode when all the supplies and references have settled to the required accuracy."
As expected, i s…