Part Number: ADS8678 Hi there,
I noted on the ADS867x datasheet as well as in the ADS8678EVM-PDK that there is no reference to or design information for common mode filtering. Is that because there is little benefit for this device? In my application…
Part Number: ADS8678 Hi there,
I am wanting to use this part for a current sensing application of 0-9V range with current sensing of 0-3A (0.3 ohm resistor). I understand due that due to the non-differential architecture the common mode voltage would…
Part Number: ADS8678 Other Parts Discussed in Thread: ADS8688 Hi Team,
Greetings!
I need your help for our customer. Is there any available example of C code for ADS8678. It will be working with Pic18F45k22 8 bit SPI.
Looking forward to your response. Thank…
Part Number: ADS8678 Hi,
I am facing some confusion while going through the specification of TI ADC (MPN ADS8678).
1. There are 8 ADC channel ( with Associated PGA), what is the AUX_IN terminal in the IC. Is it the ADC without PGA?
2. For each Analog…
Hi Charles,
You can send me a direct message - send a friend request and we can chat offline. Also, just wanted to make you aware that the TLC3578 is going on 'last time buy', so if you are committed to long term availability, you might consider changing…
Other Parts Discussed in Thread: ADS8678-SEP Hi,
Last September, you presented "Space EP Devices Planned", and in this presentation, there is ADS8678-SEP planned for Q1-2019.
Can you tell me where is this component please ? and can you send…
Part Number: ADS8678 Hello,
The ADS8678 datasheet specifies that "The PGA also adjusts the common-mode level of the input signal before being fed into the ADC to ensure maximum usage of the ADC input dynamic range.". However I do not see the maximum…
Part Number: ADS8678 Other Parts Discussed in Thread: ISO7141CC ,
Dear Technical Support Team,
Do you have a data of sink current(Io) vs Vol level ?
Datasheet describes that Vol = 0.2 × DVDD V when Io = 500-μA sink.
So if DVDD = 5V, Vol = 1V on…
Other Parts Discussed in Thread: ADS8688 , ADS8664 , ADS8674 , ADS8684 , ADS8684A , ADS8694 , ADS8668 , ADS8678 , ADS8688A , ADS8698 Hi ti
Could you help to provide some ADC chipset with linux driver(better to have linux source code)? CPU is am571x。
spec
14bit…