Part Number: ADS8686SEVM-PDK Other Parts Discussed in Thread: ADS8686S Hello,
I tried to capture signal and see on GUI, I used one of the analog channels and send 20 mVpp - 200 mHz sine signal, but i have just read 0V on analog channel AIN0 on GUI, after…
Part Number: ADS8686SEVM-PDK Hello Selected to order ADS8686SEVM Does it includes the 16 channels ADS8686 board and the ADS8686-PDK PHI board or do I need to order them as two separate items. As paired they are a single item in MOUSER. 595-ADS8686SEVM…
Part Number: ADS8686SEVM-PDK
ADS8686S-EVM is used to obtain the A/D value of each CH. As a test, I am using a DC generator to apply voltage directly to each channel, but when I convert the obtained value to voltage with 16 bits, it differs from the input…
Part Number: ADS8686SEVM-PDK Other Parts Discussed in Thread: ADS8686S ADS8686S-EVM is used to obtain the A/D value of each CH. As a test, I am using a DC generator to apply voltage directly to each channel, but when I convert the obtained value to voltage…
Part Number: ADS8686S Other Parts Discussed in Thread: , TMS320F28388D Good afternoon colleagues, I am working with a TMS320F28388D microcontroller together with an ADS8686S ADC converter. I'am using the ADS8686SEVM-PDK I had problems programming how…
Part Number: ADS8686SEVM-PDK To perform A/D conversion, I manually press the reset button to reset the device. Is it possible to issue an instruction equivalent to pressing the reset button externally using SPI communication?
Part Number: ADS8686SEVM-PDK Hi teams:
I am using ADS8686SEVM to do some test. I need write C code to communicate with phi-evm-controller and get the sample data of ADC. Is there a SDK for phi-evm-controller? or a communication protocol?
Regards.
Part Number: ADS8686SEVM-PDK Other Parts Discussed in Thread: ADS8686S I'm experiencing strange behaviour when the ADS8686 is run at 1.8 V DVDD (within spec).
Some register values are read wrong (repeatable, not random) and the ADC readings are very…
Part Number: ADS8686SEVM-PDK Hi Team,
Our customer would like to connect two ADS8686SEVM-PDK synchronously using a single interface. He has 32 channels to acquire simultaneously. Will the GUI allow using two of them together using a single clock?
It seems…
Part Number: ADS8686SEVM-PDK Hello,
I have connected three different sensors to the three channels in ADS86867S EVM, in T3 block. I need to acquire the three sensors data simultaneously in the CSV file for every second. For this, I have set the following…