Part Number: ADS8694 Other Parts Discussed in Thread: ADS8688 , Hi Experts,
Our customer is using the ADS8694 chip and having a lot of trouble implementing the SPI protocol. He found a library for the ADS8688 to communicate with an Arduino and has…
Part Number: ADS8694 Other Parts Discussed in Thread: ADS8664 Hi,
We are using ADS8664IDBT in our existing design and planning to use ADS8694IDBT due to higher resolution requirement.
are these chips 1:1 compatible ? I could see pin assignments of…
Part Number: ADS8694 Other Parts Discussed in Thread: ADS8686S , ADS125H02 Hi,
Can ADS8694 be utilized for differential input?
If not, could you let me know why A_nGND can support only +/-0.1?
If there is another ADC for differential input, please…
Part Number: ADS8694 Other Parts Discussed in Thread: TM4C1294NCPDT , Hii,
I am using TM4C1294NCPDT to communicate with ADS8694, i am able to set registers and read it back but while reading analog data i am getting below data and ones check attached…
Part Number: ADS8694
Hi Dale, Cynthia an all the others knowing about the ADS8694! I am trying to use the ADS8694 in a custom board controlled by the F28379 Launchpad.
My idea was to use spi, but as I did not have any results, decided to check communication…
Part Number: ADS8694 Other Parts Discussed in Thread: TMS320F28379D Tool/software: Code Composer Studio I want to use DSP28379D to coumnicate with ADS8694 by SPI. However, I found SPI word length is upto 16 bits. While ADS8694 need at least 34 bits in…
Part Number: ADS8694 Other Parts Discussed in Thread: TMS320F28379D Dear all,
I am still having problems to use SPI with the ADS8694.
If I use GPIOs without the SPI, the ADC responds to all my commands and sends results back. All the signals are there…
Part Number: ADS8694 Hii,
I am using ADS8694 ,
When i am going to communicate this IC with Arduino, communication is happening but
when i am going to acquire the data , i am not able to get the correct data. below data is getting when i am giving…
Part Number: ADS8694 Hii,
I am using ADS8694,
When i am going to communicate this IC with Arduino, communication is happening but
when i am going to acquire the data , i am not able to get the correct data. below data is getting when i am giving…
Part Number: ADS8694 Can I use an external Vref of 2.048V (or 1.024V) with the ADS8694 ? The datasheet talks of an external Vref, but limits it to only 4.096V.
I would like to get an input Voltage range of +/- 1.28V (with a 2.048V external Vref) or…