Part Number: ADS8695 Hi Team,
There is a description show for LPF in the datasheet. The -3dB cut off frequency is 15Khz. As this device speed could be reach to 500Ksps, for signal above 15Khz, does it will be affected by the LPF? For example, customer's…
Part Number: ADS8695 I used ADS8695 in my DAQ system. After my test, I found a problem: The ADC value is bigger than the set point value.
The test data is below:
Set value ADC value ADC value to calculation
0 0 0
4.183…
Part Number: ADS8695 Other Parts Discussed in Thread: ADS8681 Dear
Customer ask whether we have SPI example code for ADS8695 can be their reference? Thanks.
They meet a issue that whatever they set the ADS8695 register value, the read sample value always…
Part Number: ADS8695 I am using ADS8695 in my project.
2. The IC is functioning properly at room temperature. But when i am soaking it at 71 degC, the outputs are getting stuck to their higher values (approx. double of the input). In this case inputs…
Part Number: ADS8695 hello,
the read command is 11001_xx_<9-bit address>_00000000_00000000,
but i can't find the introduction of the data register int the datasheet,
how can i read the data from ads8695?
thank u.
Part Number: ADS8691 Other Parts Discussed in Thread: ADS8695 , ADS8699 , ADS8681 Hello,
is there an IBIS model available for the ADS8691?
or the ADS8695?
or ADS8699?
Regards, Niels
Hi Darren,
For table 6, the input alarm flag D[9:7] should be corrected to D[9:8], this is a literal error and should be updated in the future.
A same table in ADS8695/8691 datasheet is correct, these are ADCs in the same family, FYI:
The table 7 is…
Part Number: ADS8689 Other Parts Discussed in Thread: OP07 , ADS8695 There is a 10% error in the data obtained from the output of ADS 8689. Is there any cause?
The initials are set to unipolar 0V ~ 10V. After sending the command [32'b1101_0000_0001_0100_0000_0000_0000_1001…