Part Number: ADS8860 Hi,
I use ADS8860 in my PCB. Most of time the reading is as OK as expected.
However, occasionally the two-bytes result is completely 0; and once it occurs, it remains 0 forever until I reset the whole PCB.
Can anyone enlighten me…
Part Number: ADS8860 Other Parts Discussed in Thread: ADS8861 Hi team,
We can saw that our ADS8860 is for single-ended input.
But the pin have AINN & AINP, is that means this device can also use for differential input?
Which one do we recommend?
…
Part Number: ADS8860 I have two questions regarding to 8860 reading
1. According to data sheet, it is a 16-bit ADC. But nowhere can I find info on how to convert 2 bytes to voltage. The following is how I do conversion:
adc_8860_val = a_SPI1_3_RxBuf[0…
Part Number: ADS8860 Hi Team,
I would like to ask for clarification for this video slide-7, how is it estimated that 130MHz BW is required for op-amp if no charge bucket filter is used?
Here is the video link: training.ti.com/ti-precision-labs-adcs-introduction…
Part Number: ADS8860 Dear team,
In the datasheet of ADS8860, It mentioned that the UGBW of the ADC driver should be 4 times larger than then 1/2piRfltClt, which is also mentioned in training video "The Math Behind the R-C Component Selection TIPL 4406…
Part Number: ADS8860 In my application, five or more sensors are required to sample at the same instance (audio frequency single-ended). Reference Figure 58 in the datasheet. If I use five ADS8860, the DOUT frame size of 5 x 16 bits = 80 bits at an SCLK…
Part Number: ADS8860 Hi expert,
please see below diagram in datasheet:
It is very clear:
"tconv" means period of sampling, sample-hold capacitor charging and data converting.
"tACQ" means period of communication of digital code by series…
Part Number: ADS8860 Hello TI Team
Hello,
I am Dhiren presently working on 16Bit ADC ADS8860 which is interfaced with msp430 on its SPI lines of UCA2. I am using 3-Wire CS Mode Without a Busy Indicator where DI pin of ADS8860 is pulled up to DVDD using…
Part Number: ADS8860 Other Parts Discussed in Thread: OPA320 , REF6033 Dear Sir,
I would like to know how to interface with MEMs vibration sensor (ADXL1002z) and ADS8860 single ended 16 bits ADC, and micro-processor (ESP32). Please refer to below schematic…