Hi @ Raymond Zhang1
Finally we did successfully Read and Write operation in Registers over SPI with 8 bit transfer SPI MCU.
I think if we have a lower bit transfer SPI MCU that is not a problem to communicate with higher SPI frame of peripheral.
what…
Part Number: AFE031 Other Parts Discussed in Thread: C2000WARE , Hello,
One customer used AFE031 connected a non-C2000 series chip , the initialization is complete in accordance with the example boostxl_afe031_f28379d_dacmode in C2000Ware. The SPI…
Hi Raymond Zhang1
In AFE031 support 10 bit data transfer in DAC register, I accept. But if we are sending data as 16 bit data over DAC ,that will only make sense of the first ten bits transmitted (the 10 most significant bits) and discard the remaining…
Part Number: AFE031 Other Parts Discussed in Thread: AFE030 , THVD8000 , AFE032 , Hi team,
I have a customer asking if we have any "chips for doing low data rate power line communications over 5 volts DC" that's one-way and in a smaller footprint. I saw …
Part Number: AFE031 hello. We are developing using AFE031.
1. What is the BPS of SPI communication? In which document can I find this information? The comments in the example code are confusing. I would like to see the SPI protocol documentation.
2. Is…
Part Number: AFE031 We are having the exact same issue as the Original poster of the thread "AFE031: AFE031 powerline communications (PLC) analog front-end, FAILURE" The thread was locked and no further info was given on the resolution. Could…
Part Number: AFE031 Hi Team,
I see there is reference design on PLC lite using AFE031. my customer have interest on this solution.
TI PLC Development Kit Reference Design
just want to check if there is new gen of AFE031 for this application. Thanks. …
Part Number: AFE031 Other Parts Discussed in Thread: AFE030 , AFE032 Dear forum: I have a related question here in the specific case of an AFE031 based system. I am sorry if it seems like I am repeating this from a previous thread, but some stuff is still…
Part Number: TMS320F280025C Other Parts Discussed in Thread: AFE031 Hi
I am going to use AFE031 for my project with using EABI output format.
However, it is legacy format in TI code. Please advise how to get a library in EABI formation
Thanks