Other Parts Discussed in Thread: AFE5809 , ADS1191 hello all,
I'm new to medical US, my target is to write FPGA for AFE5809, getting data from AFE5809 and putting it in some register for DSP.
as I understood this is LVDS signal, so I made an LVDS…
Dear Olu,
Could you please share your C code? As you know, I'm also in desperate need to initiate my AFE5809 EVM using OMAP L138 LCDK.
I could modify your code for OMAP L138 LCDK.
Your help means a lot to me. Thank you :)
Hi
The USB will still connect as it is powered on USB power. Can you measure the voltage on both sides of F1? This will indicate if the fuse is still intact.
Also all of the regulator are enabled by SW7 (toggle on the edge of the board). It is possible…
Other Parts Discussed in Thread: AFE5809 We would like to develop a sonar system as a fish finder. We would like to generate and transmit the wave, receive the echo of the wave after hitting an object. In the future, we would add a touch display and show…
Part Number: AFE5809EVM Other Parts Discussed in Thread: AFE5809 I interfaced the AFE5809 EVM board with KC705 FPGA board with the help of ADC-FMC Adapter board. But I have to deserialize the LVDS interface in FPGA. I tried to convert the differential…
Hi David,
Yes, here are the examples if Trigger is applied or not.
1) When we are running decimation with using trigger signal,
we can receive Sync word signal on the captured raw data.
This can help hardware and software to capture data and process…
Other Parts Discussed in Thread: AFE5809 , AFE5809EVM I am having issues getting the test generation pattern to output anything on the LVDS lines. We are using our own board design, not an EVM. Here are our conditions:
- 5V, 3.3V, 1.8V supplies are…
Part Number: TSW1400EVM Other Parts Discussed in Thread: AFE5809 , AFE5809EVM Hi,
I'm having issue with AFE5809 + TSW1400EVM board. I not able to capture waveforms. Installation of board GUIs, cable drivers are done. Power supply is also been given…
Other Parts Discussed in Thread: AFE5809 Hi,
I am working on a design with the AFE5809 and I see an odd behaviour regarding TX_SYNC_IN and the synchronisation word.
The FPGA interface with the AFE5809 is very similar to the one used on the TSW1200…