Hi Swati,
How are you?
Thanks for using AFE5809EVM and TSW1400EVM.
1) First, if you need to use External Clock source to generate different sampling frequencies
for AFE5809 ADC's Input clock,
then according to the AFE5809 data sheet, this sampling…
Hello Tessin, You should not provide +/- 6V to the AFE5809EVM. Regarding question #2, is there any particular reason why you are planning to operate the EVM this way? I will check the programmability of the field in the GUI and will get back to you.
Hi Bob,
After looking into that TI website,
then please see the following the link below:
=============
Design files (6)
and then click on:
TIDA-00419 CAD Files (AFE5809EVM)
=============
Then you can find lot of files including schematics and…
Update:
I would like to elaborate the issue, so hopefully someone can suggest a solution.
We would like to initialize our AFE5809EVM without using the AFE5809EVM GUI. The reason is that, we would like to use this AFE in our own product. As you know…
Hello Feng,
Trigger signal is not mandatory to capture data or monitor the clocks.
Your register settings seem valid and moreover if you are getting the data clock, you should be getting the frame clock as well.
You could also validate your register…
Hi Tessin,
How are you?
Thank you for using AFE5809EVM and TSW1400EVM.
You mentioned your sampling clock frequency=10MHz
and the input signal (beat frequency)=100kHz (very low input frequency). Right?
Could you please confirm this?
If this is correct…
Other Parts Discussed in Thread: AFE5809 , AFE5809EVM Hi, TI experts:
I am using the AFE5809 to design one project. I found there're lots of registers inside the datasheet.
i found one tool named as AFE5809EVM GUI, while the prerequisite is the EVM…
Part Number: TSW1400EVM Other Parts Discussed in Thread: AFE5809EVM I have encountered the following error when interfacing AFE5809EVM with TSW1400 EVM. I have checked the LED's on the TSW and the LED4 doesnt seem to glow and LED3 is glowing but it has…
Hi,
when trying to use AFE5809 device,
since this device is focusing on all the details for applying ultrasound implementation,
all the information if not clearly covered by SLOU338 file
and Tidu702 file, the customer must focus on the AFE5809…
Part Number: TSW1405EVM Other Parts Discussed in Thread: AFE5809EVM Hello,
when I evaluated afe5809evm using tsw1405evm, I found that only ‘1W_SERIAL.SVF’ is available in the firmware. Now I want to develop a new firmware for myself to use. Who can…