Part Number: AFE58JD28 Hey Data Converters team,
I have a customer prototyping with the AFE58JD28 for a project and we were hoping you could help to provide guidance on how to properly synchronize two together. Please see a summary of our inquiry below…
Part Number: AFE58JD28 Refer to "Table 9-18,as marked in the red box, DECIMATION FACTOR=6, 8ADC PER LANE MODE is also supported? Then, there is no 160X/80X/40X/20X mode similar to that described in AFED8JD48 in the AFE58JD28 data sheet. I don’t know…
Part Number: AFE58JD28 Does the following scenario support JESD 2 lane mode?
a.)MIXER enable, Decimation =3, Fs=40M
b.)MIXER enable, Decimation =6, Fs=80M
I have not seen any similar examples in the manual. If so, can you explain the settings?
Thanks…
Part Number: AFE58JD28 Hi Team,
Customer is evaluating our AFE58JD28 in their project, and having below questions about this part, can you help to check and give us some comments?
Per datasheet spec requirements as below snapshot, if we use 80MHz ADC…
Part Number: AFE58JD28 Hi Tier
My customer use AFE58JD28 to do Power-down function and wake up then go to the power-up recovery phase.
They found the AFE58JD28 do not wake up during 15ms.
So we would like to understand the detail:
1. What is the maximum…
Part Number: AFE58JD28 Other Parts Discussed in Thread: OPA2209 I tried to configure the circuit to have a range of -0.4 V to +0.4 V in CVNTLP, VCNTLM. However, the circuit is not working.. U18's OUTPUT does not change even though the DAC OUTPUT value…
Part Number: AFE58JD28 Other Parts Discussed in Thread: AFE58JD48 , Hi
I would like to ask you to support device selection.
My customer is using AD9670 as trial product.
Now they have begun to select TI's AFE to make new trail board.
I would like to…
Part Number: AFE58JD28 Hi ,
I iam using AFE58JD28 with TGC mode:
LNA(dB)
DIG_TGC_ATTENUATION(dB)
PGA(dB)
15
24
18
CLAMP LEVEL= 2.24Vpp
LPF_PROG = 20 MHz
LNA_HPF_PROG = 100KHZ
with input signl of :650KHZ pulse (30 pulses), unfortunately the max ADC…
Hi Zhihong,
My apologies for not getting back on this E2E.
Somehow this thread was missed and I am really sorry for missing your reply.
So, about the bandwidth requirements on the external amplifier, there is no compulsion to use such high bandwidth…