Part Number: AFE7222 Other Parts Discussed in Thread: TRF371109 , TRF371135 , , TRF370333 I have a query regarding the connection of IQ outputs from TRF371109 and TRF371135 to form a single IQ channel (one differential I and one differential Q) for sampling…
Hi Mike,
I have received no new information from my team at this moment, but we are working on contacting one of the parts designers for more information.
Regards,
David Chaparro
Part Number: AFE7222 The datasheet for the AFE722x family specifies the ADC's input DC resistance at >1MOhm in parallel with 4 pF. What is the differential input impedance (e.g. 50, 100 Ohms). The datasheet doesn't specify if the inputs are buffered either…
Part Number: AFE7222 Other Parts Discussed in Thread: AFE7225EVM , TRF370333 Dears.
customer is developing AFE7222.
AFE7222 DAC has a current output, but use Voltage input GRF6413, need Current to Voltage with Common voltage tuning. Use Transformer or…
Part Number: TMS320C6748 Other Parts Discussed in Thread: AFE7222 , , TMDSLCDK6748 Hello! I want to try using IF tranceiver AFE7222 with DSP TMS320C6748. If I right understud the best way to connect is use uPP interface to AFE. I have some question:
1.…
Part Number: AFE7222 Other Parts Discussed in Thread: TRF370333 , Hello!
I have question regarding connection of baseband signal to quadrature modulator/demodulator. In PCB mounting the IC have several layout, and I can't connect output of demodulator symmetrical…
Part Number: AFE7222 Hello,
Make AFE7222 schematic as attached.
And there are 2 or 3 options for Tx & Rx path.
1. Tx Path : will use default path(Resistor path) if there is no problem.
two other options(RF Transformer path & Capacitor path…
Other Parts Discussed in Thread: AFE7222EVM Hi all,
1. I would like to know, is there anyway to connect AFE7222evm with PC without any FPGA device,(using uPP )
2. Is there any way to connect MatLab Simulink direct to AFE7222EVM?
Thanks ,
Sargis Sargsy…