Hi Zoran,
This alarm may be signaling that the ADC input is being overdriven. Can you try decreasing the input level to the ADC? You can also try increasing the DSA on the either the Tx or Rx side so that the amplitude is decreased.
Regards,
David …
Part Number: AFE7444EVM Other Parts Discussed in Thread: AFE7444 , AFE7900 , AFE7950 Hi Ti Team,
I am looking for AFE7444EVM design file, please point me the schematic.
Thank you, Best regards, Alder
Part Number: AFE7444EVM hi Everybody,
I have been using AFE444 EVM for about 6 months now. In the last two weeks, the board have developed a new behavior which affects the phase of the signals. To be more precise, the phase between the signal input…
Hi Zoran,
Wer recommend updating the mapping in the FPGA. Can you share the pin assignments for the SerDes lanes in your design?
Regards,
David Chaparro
Hi Wanrui,
If the e-fuse is not loading correctly then there are a couple of things that could be the cause.
Please check the following:
1. A stable clock should be provided to the AFE before the e-fuse loading. Has it been verified that the clock is…
Part Number: AFE7444EVM Hi TI team,
Greetings for the day.
I want to use the AFE7444EVM with ZC706. Does Ti provide the reference Vivado project?
Thank you.
Part Number: AFE7444EVM Other Parts Discussed in Thread: AFE7444 HI
I am using AFE7444 EVM. I generate a signal for my experiment and send using the AFE7444 board. I was able to capture, but I noticed two small signal components on the side of the spectrum…
Hi Zoran,
We have tested the Mode 6 configuration on our side and we notice that when after pressing Run Complete Startup Sequence the PLLCLKLD and PLLREFLD LEDs turn on. One thing to check for this is to make sure that AFE power supply is set to 5V and…
Hi Hao,
In AFE7444 secure folder, there's a JESD reference design for KCU105. You can use this as a reference to create a design for ZC706 or other Xilinx FPGAs. This old design is based on Xilinx JESD204 IP. You can access the secure folder at: …
Part Number: AFE7444EVM Hi TI team,
Greetings for the day.
I want to use the AFE7444EVM with ZC706.When I plug the AFE7444EVM into the ZC706 HPC FMC interface, vivado can't detect the device. When I pull off the board, the error disappears.
Waiting…