Part Number: AFE7769 Hi WI Team:
I want to configuration AFE7769 in Latte.
a). I haved executed setup.py.No error appears
b) I'm executing devInit.py. Error appears. Couldn't load iGUI.
c). I'm executiing basicBringup.py. Error appears. SPI…
Part Number: AFE7769 Hello,
We are working on our custom SDR
Our radio engineers have chosen a chip for our devices.
It will be AFE7769.
They ask if you can provide "S-parameters" files for AFE7769 RF in/out ports?
Could someone help me…
Part Number: AFE7769-3P5EVM Other Parts Discussed in Thread: TSW14J58EVM , AFE7769DEVM , AFE7769D Tool/software: Can I get a user guide to interface AFE7769D-35EVM with TSW14J58EVM.
I searched over TI website, I could find the below document
1) Interfacing…
Part Number: AFE7769 Tool/software: When the TX_PLL of AFE7769 is set at 880MHz, a large power DC will be generated, and the QMC automatic calibration cannot go down, affecting the ACPR, this problem has a small probability, about 1/250, help to analyze…
Part Number: AFE7769-3P5EVM Tool/software:
The errors I am getting are
1) AFE configuration in progress.
2) Could not detect FPGA Reset FTDI, Please reset FPGA manually.
Thanks and Regards,
Kalyan Giri
Part Number: AFE7769 Hi, We are using AFE7769 in our design as per out layout requirements we are Planning to place SSRF section in the following manner..
We are Planning to give isolation with shield on TOP and Bottom i.e (for TX & RX ) And ORX signal…
Part Number: AFE7769-3P5EVM Other Parts Discussed in Thread: AFE7769D Hi WI team,
AFE7769-3P5EVM Latte version I have is 0p3.
Do you have updated AFE7769D Latte version?
I faced some board connection error in my customer side, therefore I want…
Part Number: AFE7769EVM Other Parts Discussed in Thread: AFE7769 , , AFE7903 We have a problem with Latte for AFE7769. After installation TILatteV5p2p3.exe we do not see any .py files in the "project" folder. So main Latte window does not show any information…
Part Number: AFE7769 Hi Team,
When doing temperature compensation on AFE7769, we found that there was a problem with the attenuation accuracy of RX. When the attenuation was 1dB, 2dB, or 3 dB, the error was negligible. But when the attenuation was…
Part Number: AFE7769
Hi Team,
The shared international repeater project currently uses an AFE7769 (4T4R2FB) and an SN18064 (4T4R1FB). There are problems with the channel 3/4 of SN18064
SN18064’s problems: it’s under the 4TR, dual sync mode…