Part Number: AM3352 When booting from SPI Flash memory, a glitch waveform appears in CS and CLK before SPI read access starts. This waveform may cause the Flash memory to go into a busy state.
Please tell me the cause of glitch waveform and how to prevent…
I reviewed the spreadsheet that was sent. Step 3 and 5 says to write to the MAIN_RST or DMA_RST and CORE_RST, but it appears that you are doing both.
You should either do line 1722 and 1729 (remove 1720,1721,1727,1728)
OR
keep 1720,1721,1727,1728 and…
Part Number: AM3352 Hi,
We are using the AM33 processor P/N: AM3352BZCZA100 which does not support Secure boot (HS version).
Can you help me with the below questions? - What is the matching P/N to have HS supported? - What Linux Kernel supports the HS version…
Part Number: AM3352 Hi,
1.What is the IoL(Max) of AM3352 LVCMOS pin in the picture below? (VDDSHVx=3.3V)
2.What will be the impact if the actual measured IoL=7.3mA exceeds 6mA?
Part Number: AM3352 Other Parts Discussed in Thread: TPS65910
Hi Support Team,
The following voltages are applied to the VDDSHVs of AM3352.
VDDSHV1,2,5: 1.8V VDDSHV3,4,6: 3.3V
3.3V is taken from a different IC from TPS65910, The rise time of 3.3V is about…
Part Number: AM3352 Hi,
I would like to know about the settings of the AM3352's PLL and LCD controller. Can I ask a question via private message as it contains confidential information?
Thanks,
Conor
Part Number: AM3352 Error in the log:
sdk9 make uboot.log
tony@ubuntu22:~/ti-processor-sdk-linux-am335x-evm-09.01.00.001$ make u-boot
===================================
Building U-boot
===================================
mkdir -p /home/tony…
Part Number: AM3352
Hi sir,
We are using a custom board with AM3352 and we have a HF RFID Desktop USB Reader (RRHFOEM07) from RapidRadioSolutions and when it connects , it connects as hid-generic. How to communicate or read from rfid by hid-generic connection…
Part Number: AM3352 Hi Champ,
I am asking for my customer.
They have used AM3352 on MP product for several years, this time there is a failed return reported by customer.
So far, customer has only seen one piece from thousands of unit happening such issue…
Part Number: AM3352
Dear Champs,
I am asking this for our customer.
The user wants to do USB2.0 Host & Device Mode Compliance Test.
The user uses Linux SDK.
Would you please provide the corresponding Command or other method to implement into USB…