I guess what I'm saying is, the linux documentation make use of a complete different method that does not seems to work. see Linux TILCDC panel
And the TI documentation does not mention anything other than HDMI see AM335x LCDC DRM Display Driver
The…
Part Number: AM3358 I'm working on a bringup for meta-flutter on the beaglebone black DRM backend.
First pass is with core-image-weston. Weston fails to initialize with:
Mar 30 09:44:24 beaglebone weston[490]: [09:44:24.-1097469832] EGL error state…
Part Number: AM3358 Hi Champs,
I'm trying to follow the steps in link below:
https://software-dl.ti.com/processor-sdk-linux-rt/esd/AM335X/09_01_00_001/exports/docs/linux/How_to_Guides/Board_Port/U-Boot.html#overview
to build the u-boot for a custom…
Part Number: AM3358 Hi,
The BBB board has a LAN8710A PHY connected to the processor AM3358. I'm trying to access the Ethernet PHY register available on BeagleBone Black board. I am not using so I want to disable this PHY, ultimately some power will…
Part Number: AM3358 Hello,
I need to get an TI Representative to send us the documentation for the AM3358 crypto processor. We are USA-based company and we should already have an NDA with Texas Instruments.
Thank you,
andy
Part Number: AM3358 During bulk transfer mode some packet get lost on call of USBBufferWrite(const tUSBBuffer *psBuffer, const unsigned char *pucData, unsigned int ulLength) function.
Part Number: AM3358 Other Parts Discussed in Thread: AM3357 Hi,
Q1. I'm considering using Gigabit Ethernet with the AM335x. Am I correct in my understanding that if I want to perform 1 Gigabit communication with AM335x, I need to use a model number with…
Part Number: AM3358 Hi, I get this error when trying to interface SLB9670 with BeagleBone Balck over SPI1, bus with CS1:
tpm_tis_spi: probe of spi1.1 failed with error -110
This is my overlay:
/dts-v1/; /plugin/;
/ { compatible = "ti,beaglebone","ti,am335x…
Part Number: AM3358 Other Parts Discussed in Thread: TPS65217 Hi,
I am bringing up a new board based on the Beagle Bone Green Wireless (BBGW). The power rails are all as expected but the MCU does not want to boot from the uSD card interface. One of the…
Part Number: AM3358-EP I am using ti-processor-sdk-linux-am335x-evm-09.01.00.001.
While building kernel I'm getting fatal error: gmp.h: No such file or directory
Commands executed are:
make ARCH=arm CROSS_COMPILE='arm-none-linux-gnueabihf-' multi_v7_defconfig…