Part Number: AM3359 Hi Team,
I am trying to flash the board. I have loaded isdk_spi_flasher.out file . I have successfully flashed and i change the jumper pins 2 & 3 and i started the board. Issue : The voltage is not stable it is decreasing. solve…
Part Number: AM3359 Other Parts Discussed in Thread: SYSBIOS Hello
I have a question. I try to run Ethernet/IP adapter example on Am335x icev2.1 board. I am not able to ping this board from my PC.
1. when I use these
PRU-ICSS-EthernetIP_Adapter-01…
Part Number: AM3359 Hi team,
I am working on the Am3359 board. Now I have created 2 rootfs and 1 boot file on the SD card, and I am trying to switch between the two rootfs by changing the extlinux.config file. While booting, it is asking and by keyboard…
Part Number: AM3359 Other Parts Discussed in Thread: AM3356 Hi,
I was trying to use L2 cache lockdown feature to run critical code and data from locked down cache.
I have gone through cache lockdown code from Cortex A8 symbiose code.
When I am running…
Part Number: AM3359 Hi there,
I am trying to create an yocto image and have an application which needs to be compiled with arm-linux-gnueabihf-gcc compiler.
The current yocto setup is generating the arm-poky-linux-gnueabi-gcc compiler.
I tried few things…
Finally, to compile de Kernel I need to add this depends on $PATH:
export PATH=/opt/ti9/external-toolchain-dir/arm-gnu-toolchain-11.3.rel1-x86_64-arm-none-linux-gnueabihf/bin:$PATH export PATH=/opt/ti9/linux-devkit/sysroots/x86_64-arago-linux/usr/bin:…
Hi Himanshu,
Thank you for the detailed reply. I have managed to enable VLAN tagged PRP SV frames. We encountered an issue with root file system mismatch. We were using a previous version of RFS while the SDK was 6.1. We didn't switch to the corresponding…
Part Number: AM3359 Other Parts Discussed in Thread: SYSCONFIG Hi,
I created my devicetree.dtsi from sysconfig application. I created this config from AM335x ZCZ:
DCAN1 -> UART0
GPIO -> GPIO0
LCDC -> LCDC
ETH1 -> GMII1
ETH2 -> GMM2
UART…
Part Number: AM3359 Hi TI team,
I am facing an issue while defining the GPIO direction as output. I am using GPIO2_5 as the LAN PHY reset, which is one of the inputs of the 7UL1T80FU AND logic IC. This pin operates at 1.8V, while the second input and…