Part Number: AM3359 Hi TI team,
I am using AM3359 TI processor for our application .
I am working on GPMC protocol,where I have .ko file based on Our Custom board version.
Custom Board version Kernel is --- 4.19.94
for Custom Boards we have generated…
Hi Priyadharshini,
Baremetal examples are provided in the PROCESSOR-SDK-RTOS-AM335X downloadable in the link below. Please check if the package provides what you need.
https://www.ti.com/tool/PROCESSOR-SDK-AM335X
Part Number: AM3359 Hello We have a custom Sitara board with a broadcom 548xx gigabit PHY. It's using the RGMII interface with the Sitara.
When we boot the board with the Ethernet cable plugged in to a PC, the connection is set up correctly at 1Gbps…
Hello Ken,
Thanks for the additional information. Please refer to this application report: https://www.ti.com/lit/sprac32 . This report was based on earlier versions of the SDK, but the general principle should apply to the latest SDK. Please also look…
Part Number: AM3359 Hey folks, I am currently trying to generate a PWM signal using the ECAP as an interrupt timer signal. I have found the following code which I am trying to adapt:
gist.github.com/.../6aa3d90fa7cfc6df06118360b67b48da
The problem here…
Part Number: AM3359 Other Parts Discussed in Thread: SYSBIOS We are having problems to handle exceptions correctly since we have migrated to gcc and SysBios 6.76.03.01. A System_printf in Exception_excHandler is causing another exception which overlaps…
Hi Adam,
we were just going through our issue backlog and noticed this issue/ticket here is still open. Do we still need to investigate this further, or has there perhaps been some progress/resolution that we can record here?
Thanks, Andreas
Part Number: AM3359 Hi,
I have customers using AM3359, now some questions, please help to answer.
1. Must the two pwm channels in ehrpem0A and ehrpem0B in eHRPEM be set to the same period?
2. PWM operation generally use file access Such as/sys/class/PWM…