Part Number: AM3871 We are having an issue with video from the AM387x. After several hours the output from the AM387x turns black. The video control signals, VYSNC, HSYNC and pixel clock are running correctly. The video pixel data is set to 0. On our…
Part Number: AM3871
Hi TI experts,
In some situations, it is required to separate Analog and Digital ground when using mixed signals. Based on what is written in the AM3871 specification, I see that this is not required.
1. I want to understand why this…
Other Parts Discussed in Thread: AM3871 , TPS51200 Hello TI Experts,
I studied a few notes on the DDR3 memory layout from TI (SPRABI1C), NXP, Micron, Xilinx, and other manufacturers, and I had some questions:
1. To which signal group does the DDR3.RESET…
Part Number: AM3871 Hello, I need to interface with a Compact Flash and am asking how that is done. I've read that you can interface with Compact Flash using the EMIF interface. Also, I am needing to use the CFAST 1.0 spec which supports I believe 300MB…
Other Parts Discussed in Thread: AM3871 Dear Support Team,
We have a device based on AM3871 (AM3871CCYE80-ND) CPU and there is a task for our product to be certified (to obtain CE and FCC sign).
The CPU we are using has a marking - Contains lead / RoHS…
Hello Sebastian Graf,
Thank you for the query.
I did a quick check internally if there are any recommendations or documents for interfacing AM335x GPMC to a compact flash card.
I could not find any information that i could share.
Please check if the below…
Other Parts Discussed in Thread: AM3871 Hi,
I am designing a custom PCB which has AM3871 on it. We are not planning to use any audio or video functionality and so don't have a need to add the additional crystal or a oscillator to source the AUXOSC_MXI…
Other Parts Discussed in Thread: AM3871 Hello,
1. Can you please let me know what is the offical RTM (production) date of AM3871?
2. Are samples available?
Thanks
Piotr
Other Parts Discussed in Thread: AM3874 My company has created a product using the AM3874/DM8148 chip. I've got u-boot in nor and booting from it. I'm now working on the kernel. I'm now at the point where I'm trying to get the NOR flash supported in the…