Part Number: AM4382
Hi Team,
I wanted to simulate Signal integrity with TI's available IBIS file AM438x.IBS, while selecting USB0 and USB1 pins in model these USB pins only shows "INPUT" option only we not able to find driver/output option here in models…
Part Number: AM4382 Hi,
This is Pankaj from eInfochips India and I am currently working on AM4382CZDNA30S Processor Based Project which is used for EPOS application and we are using TPS65218D0RSLR PMIC with the AM4382CZDNA30S Processor and my system is…
Part Number: AM4382 Hi,
Here, We are attaching a USB device to am438x epos evm Board on usb type A host. And we are getting log as follow.
usb usb1-port1: Cannot enable. Maybe the USB cable is bad? usb usb1-port1: Cannot enable. Maybe the USB cable is…
Part Number: AM4382
Hello Sir,
I refer AM438X series but i need some queries regarding VDD_MPUOPP and VDD_COREOPP.
1) If i m used AM8X 600 MHZ parts so what is max voltages of VDD_MPUOPP and VDD_COREOPP. Please also tell us VDD_MPUOPP version detail in brief…
Part Number: TPS65218D0 Other Parts Discussed in Thread: AM4382 , Hi,
What is the current consumption of TPS65218 when RTC only running and powering AM4382 processor? (only Coin Cell battery power into CC pin) Thanks in advance.
ROFINO
Part Number: AM4382
Hi,
I am working on TI processor (TI438x Sitara processor) for doing such kind of below operations: 1. RSA 2048 Sign in and verification function - RSA 2048 key generation - RSA 2048 Encryption and Decryption - RSA 2048 certification…
Part Number: AM4382 Hi,
I am working on evaluation board of AM438x device. In which I am having an application which takes raw image data from USB and displays on screen.
For this I had used QT 5.9.16.
This system is running over 600 MHz.
Image is comes…
Part Number: LINUXEZSDK-SITARA Other Parts Discussed in Thread: TCA5013 , AM4382 , TRF7970A ,
We are evaluating the Platform to be used for the design of a POS Terminal (for Toll Gate Payment) performing both Contact & Contactless and NFC payment transactions…
Part Number: AM4382 Other Parts Discussed in Thread: SN74CB3T3257
Working on Costing for the New Product development
Product Requirement : Plan to use 2 Separate camera in Single parallel Bus for the Different application
Pls advice can i do interface…