Hi,
Ethan Tian said: We modified the strap mode of phy to match with the phy ID modify
Does this mean there are some hardware changes? or do you change the strap register post PHY reset?
Regards, Tanmay
Part Number: AM5716 Other Parts Discussed in Thread: TMDXIDK5718 , SYSCONFIG , Hello,
I'm working on a Sysconfig for a custom board using the AM5716 Processor and wanted to verify the generated file process. For some background we've been using the TMDXIDK5718…
Hi Darren,
This may be related to TLP, mainly because the nature of that errata is when a message that is shorter in length than 4 bytes is sent, the message automatically gets aligned to 4 bytes. Since the receiving end expects only 1 byte but receives…
Part Number: PROCESSOR-SDK-AM57X Other Parts Discussed in Thread: TPS65916 , AM5716 , TPS659037
Same question as I linked. I am trying to get the PM driver working using a TPS65916 PMIC and an AM5716 (running on the C66 core). The driver appears to not…
Part Number: AM5716 Other Parts Discussed in Thread: SYSBIOS My goal is to build the PDK without any optimization for easier debugging. I was able to (re)build the pdk, which resulted in binaries for each package (and core) in a new 'debug' folder.…
Part Number: AM5716 Hi,
Our customer are looking for DSP processor with USB and EMAC for their application. We are suggesting AM571x and C66AK2Gx Multicore device for them and have some questions.
In a multi-core product with ARM and DSP, will each core…
Hello Zhicheng,
We have detailed brainstorm on this issue and have identified the reason why the ROM code is unable to detect the newly written MLO file after certain amount of reboot.
The reason is that the fat driver part of the eMMC boot functionali…