Part Number: AMC1100 Hello,
What is the technology of the AMC1100?
Do you get a photo of the AMC1100 internal construction (position of die)?
Thanks a lot beforehand.
Part Number: AMC1100 Other Parts Discussed in Thread: ADC161S626 , OPA2388-Q1 Hi,
I've chosen an operational amplifier (opamp) that can convert a 10V analog signal to a lower voltage, which will be fed into an isolated differential amplifier. The resulting…
Part Number: AMC1100 Hi, i'm using an AMC1100 upstream of an ADC for sensing and need accurate gain and output phase values for it to account for them in the ADC. In Tina i've simulated the spice model and it gives me around -0.06 degrees phase shift…
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1200EVM , AMC3301 Hello everyone,
I am controlling the speed of an AC motor using a dimmer, but I want to be able to measure the AC voltage of the motor, I thought about using a current transformer…
Part Number: AMC1100 Customer has concern about SER.
And then I showed TI standard the below.
・SER, is reported in FIT or FIT/Mbit (when focused on memory).
But The customer was not satisfied with TI standard.
Could you give me SER ? or How should I reply…
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1300 , AMC1200
Hey team,
My customer, Milan @ Eaton, is looking to use the AMC1100 and is wondering if there are any tolerances he may want to consider when calibrating at 25degC only . This is for…
Part Number: AMC1100 We are a TI part user and OEM customer.
We have implemented API V1 last April, 2022 and are happy about it.
However, this morning, when trying to order AMC1100DUBR, I have received a component order failure message.
I used to be able…
Part Number: AMC1100 Dear Team,
I'm using the AMC1100 Isolation Amplifier for DC Voltage sensing,
I need to design the Circuit suitable for Insulation resistance at 2000V, With shorted the all terminals with body.
If I use the primary side voltage…
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1301 , AMC1200 , TLV170 , OPA350 , TLV6001 , AMC1300 , AMC1350 , AMC1351
Dear TI team,
Good evening.
We are using AMC1100 for AC voltage sensing(0-270V),DC voltage sensing(300V DC and 600V DC) and AC…