Part Number: AMC1106M05 Hi,
We are using the AMC1106M05, The maximum offset should be 50uV according to the datasheet. In some cases the offset is higher then this specification.
The temperature of the board is stable at 22'C. Both inputs are shorted to…
Sure,
From the datasheet: "The AMC1106 incorporates front-end circuitry that contains a differential amplifier and sampling stage, followed by a ΔΣ modulator. The gain of the differential amplifier is set by internal precision resistors to a factor of…
Part Number: AMC1106M05 Other Parts Discussed in Thread: TMS320F28388D , Hello,
I am struggling with the signal timing of the AMC1106M05 delta sigma modulator, together with the TMS320F28388D. In principle what I have is this:
The timing diagramm will…
Part Number: AMC1106M05 Hello Team, my customer needs support on shunt resistor configuration
Target is to achieve a measurement range of +/-350A-p (referred to +/-64mV). Shunt selection is difficult because only certain standard values are available…
Part Number: AMC1106M05 Hi,
I'm looking at the datasheet for AMC1106x and in the typical application section it shows that the shunt resistors can be connected to the hot lines.
Also in the datasheet mentions that the voltage that can be on input…
Part Number: AMC1106M05 I try to use AMC1106M05 in my design. I read though the datasheet. But I still do not know what is format of data? How do I know the start of a data, or end? How many bits of the data from DOUT?
If any info, will be greatly appreciated…
Hi Utku,
Can I ask you how much of the TIDA-01094 reference design you are using? The AMC1106M05 itself should not be causing the problem, but you can try to verify that by removing the diodes and make sure that AGND is tied back to your shunt.
I was…
Part Number: TIDA-01063 Other Parts Discussed in Thread: TIDM-3PHMETER-ROGOWSKI , TMCS1100 , AMC3301 , AMC1106M05 , Dear TI expert,
I am finding a low cost sensor to measure a low current for overlaod protection, current range from 0.16A to 5A, 50/60Hz. I would…
Hi Cody!
One of my associates is suggesting that you might take a look into the AMC1106M05. This could provide Option 3 if you have the means to filter a digital bit stream similar to what was done with our TIDA-01639 reference design. Take a look and…
Part Number: TMS320F280049 Other Parts Discussed in Thread: AMC1106M05 , AMC1106E05 Hello,
I want to perform current measurement with SDFM module and AMC1106M05 while measure voltage with internal ADC. For accurate result acquisition I need to get almost…