Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC3301 , AMC1300 Dear support,
I use AMC1200 to do current sensing in my design.
The input power of my design is DC 48V to 160V.
VDD1 & VDD2 = 5V, magnitude of current to measured =0.68…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC3301 , AMC1200EVM Hi,
I use AMC1200 to do current sensing in my design below,
The reference circuit i use was based on below isolated amplifier current sensing tables.
However even the…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , OPA350 I designed the measuring circuit with AMC1200. At input I have a peak voltage 200 mV AC. The oscillograms of the inoutmeasured exactly at the inputs of AMC1200:
Unfortunately, at…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 I am creating a six-channel sensor on 4-layer PCB with the use of AMC1200. Are there any concerns to put two devices in the same coordinates but on top and bottom layer. Meaning that die of…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC1200EVM , AMC3301 , INA236 Dear support,
I plan to use TI above 2 TI IC for current & voltage sensing in my design.
Can you help me to check with TI whether my preliminary circuit design…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 Hello TI Team,
I am planning to AMC1200-Q1 for AC Voltage Sense. Does AMC1200-Q1 support for AC voltage Sense?
If yes then,
Can you explore me the point VINN and GND1 is short?
or please…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC3330 , AMC1311 Hello TI Team,
I am planning to use this part :AMC1200BDWV for DC voltage sense.
As per datasheet,
The VIN is shorted with GND1 why?
what are the advantages and disadvantages…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC3301 Hello,
I am using AMC1200-Q1 for isolated voltage sensing.
The sense resistor across AMC1200-Q1 is 673 ohm & max drop across it is 246mV.
But, the current through it is 375uA…
Other Parts Discussed in Thread: AMC1200-Q1 , AMC1300B-Q1 , AMC1200 , AMC3330 , AMC1350 Hi team,
Could you recommend current sensing IC for output below?
This is AC output, so isolated device should be needed.
Total is 10ch. It doesn't have to be 10ch at…