Part Number: AMC1302EVM Other Parts Discussed in Thread: AMC1302 Had a question related to shorting GND1 to AINN to solve the common mode issue. I was just wondering by how much the AINP voltage can dip below the GND1 reference once the GND1 is shorted…
Part Number: AMC1302EVM Other Parts Discussed in Thread: AMC3330 , AMC1302 , AMC3302 I'm using two AMC1302EVMs to characterize a DC motor. One measures the motor voltage, and one measures the motor current. I have the outputs of the amps connected to differential…
Part Number: AMC1302EVM Other Parts Discussed in Thread: AMC1302 , I'm using this amplifier EVM to act as a current sensor by means of a shunt resistor, with the differential output of the AMC feeding into a DAQ. I'm trying to measure the current that a…
Part Number: AMC1302EVM Other Parts Discussed in Thread: AMC1302 , AMC1311 Dear TI Members,
I evaluated AMC1302EVM
I got linear output on it from 240Vac, and voltage divider 5M and 1K to the input, but the output sine is not good,
Any suggestions on it…
Part Number: AMC1302EVM Dear TI Members,
Currently I'm evaluating AMC1302EVM,
Can you suggest me how much is the value for the filter circuit in this schematic ?
Any calculations or example ? My input is maximum 260Vac and output for ADC, Vcc between…
Part Number: AMC1302EVM
Dear TI Members,
Which op-amp for signal conditioning do you suggest me for this board ?
I'm going to use it for 250V AC input and 3.3V ADC output,
Thanks and kind regards
Part Number: AMC1300EVM Other Parts Discussed in Thread: AMC1302EVM , AMC1300 , AMC1301 , ISO224 , AMC1302 Dear TI Members,
Does anyone have experience with this Evaluation Board ?
AMC1300EVM
au.mouser.com/.../AMC1300EVM
Thanks