Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311 , Hello Team,
i have a query, i need the Failure mode distribution of AMC1311 along with the FIT rate information. I couldn't find it .
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311
This is the picture of our voltage sensor model using AMC1311 for the closed loop control of boost/buck converter.
The simulation is working fine but when it comes to the physical hardware…
Part Number: AMC1311-Q1 Hi Eva,
Per talked, we can follow up below discuss here:
https://e2e.ti.com/support/amplifiers-group/amplifiers-internal/f/amplifiers-internal-forum/1346937/amc1311-q1-failure-at-350v-hv/5132402#5132402
Thank you!
Marc
Hi Frank,
Frank QIN said: Should we consider OUTx as voltage source to do the calculation?
Yes, this should be fine. the OUTx pins can drive 14mA's of current, it can be considered as a voltage source when connected to a high impedance.
Frank QIN said…
Part Number: AMC1311-Q1 hi expert
taking TCVOS as an example,
There is a comment(1) in datasheet.
do we use one standard deviation (sigma) or six standard deviation (sigma) to describe these parameters?
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC3330-Q1 , Hi Team,
Customer is design CAR OBC and using AMC1311-Q1 and AMC3330-Q1 for BAT voltage sense.
End customer request ASIL-B level for this function block. Do we have any reference design…
Part Number: AMC1311-Q1 Hi TI Expert,
We notice the VFAILSAFE(VOUTP - VOUTN) will be -2.6V if following condition is fulfilled.
Is there any way that we can keep the VOUTP-VOUTN as 0V even the VDD1 power is missing?
Or the only way is to disable the…
Part Number: AMC1311-Q1 Hello, Team,
The datasheet only specifies the failsafe differential output voltage V_FAILSAFE with a condition of VDD1. Also, 7.3.3 only mentions about VDD1 and SHTDN when this fail-safe output occurs.
Does this mean that VDD2…
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311 , Hello team,
My customer is using AMC1311.
During their test, the input terminal (Vin) of AMC1311 may exceed 2V, almost 2.15V. However, after testing, there was no problem at all temperature…
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311 Hi Expert
Do we have wafer probing for the component of AMC1311B-DWVQ1?
This component can not be used if there ’ s no wafer probing in our system.
If not, do we have alternative for…