Part Number: AMC7834 Other Parts Discussed in Thread: AMC7832 , AFE20408 , AMC7836 , AFE10004 We have used the AMC7834 extensively for power amplifier control. I am evaluating a new GaN power amplifier device which requires -5.3V negative voltage. I have…
Part Number: AMC7834 Hi Team,
May I know what is the AVDD,AVCC,DVDD power on reset threshold? I only find 4.5V in section 8.3 and 3.9V in section 6.7. Thanks. The application is apply AVCC/AVDD/DVDD=5V.
B.R.
Lucas
Part Number: AMC7834 Hi TI,
I have question that why the PA_ON pin is used to driving an external PMOS switch only, could I use the NMOS ?
I have the GAN VDD is 28V which is over the limit of PA_VDD 20V, do you have recommend PMOS switch from TI could…
Part Number: AMC7834 Other Parts Discussed in Thread: AFE10004 Hi expert,
Customer is looking for PA monitor solution and to do temperature compensation. There are three PAs in that chip and need power up sequence.
VG1/VG2/VG3 supply -5V--> VDD1/VDD2 supply…
Part Number: AMC7834 HI team,
Could you let me know the definition of the table for clamp mode?
In this table, we clamp DAC form 3.5V when it enters clamp mode. Does it mean that AMC7834 clamp DAC to 0V from 3.5V? and it takes max 5us.
Does it mean AMC7834…
Part Number: AMC7834 Hi expert,
Customer used AMC7834 and have some questions about SPI timing spec e.g. ODZ and OZD although so far no any communication issues.
What customer measured tODZ is -452ns(spec: 0-10ns) and tOZD is 20.4ns(spec:0-15ns) which…
Part Number: AMC7834 The official website only provides GUI. Do you have any C language routines for reference? It is sufficient to achieve basic functions.
Part Number: AMC7834AMC7834
Is there any ripple rejection between the AVss pin and the output of the DAC on this IC, the datasheet shows output noise from the DAC's but I am not seeing any information on ripple rejection.
I am considering a LDO external…
Part Number: AMC7834 Hi Expert,
May I clarify what's the purpose to design the stencil separating 25 windows by the vias? Or can customer just have a complete plan with vias?
Regards,
Allan
Part Number: AMC7834 Hi Expert,
In the datasheet of AMC7834, the grounds of the analog circuit and the digital circuit are separated (first picture), but they are finally connected together at a unknown position (second picture). Third picture is our circuit…